Muck Boots Peak Essential Hiker Named a Winter Essential by OUTSIDE Magazine


Peak Essential

 

Muck Boots new Peak Essential boot was honored by OUTSIDE magazine in the Winter Buyer’s Guide as an essential winter hiker for the upcoming season. The guide, which offers readers’ insight into the results of the magazine’s field-tests of hundreds of products, calls the hiker “the warmest, most supportive boot” in its category. 

The Peak Essential is a lightweight boot built with a neoprene bootie inside for maximum comfort, warmth and 100 percent waterproof protection all the way to the top of the boot.

In addition to the Peak Essential, Muck Boots’ new fall 2014 collection includes five other new boots that feature the company’s comfortable, light-weight and waterproof designs for farmers, hikers, hunters and outdoor enthusiasts of all ages.  For men, the Peak Hardcore is another lightweight waterproof hiking boot and the Pursuit Fieldrunner and Pursuit Glory are high performance boots designed for big game hunting. For women, the Arctic Adventure Zip Suede is a soft, stylish and slimming boot that is easy to slip on and features a waterproof suede upper, and the multi-season Hale boot, also available for kids, is 100 percent waterproof and lightweight with a self-cleaning ribbed outsole that provides improved stability for walking on outdoor surfaces.

Learn more about Muck Boots.