Muck Boot Company Unveils New Fall Styles With Award-Winning Hunting Boot And New ‘Diamond Collection'


Just in time for the fall hunting season, Honeywell’s The Original Muck Boot Company introduces the lace-up Pursuit Shadow, weighing in at 1 lb, 7 oz , making it one of the lightest hunting boots on the market. Despite the fact that the boot is both lightweight and packable, the Pursuit Shadow still features Muck Boot’s groundbreaking technology and signature neoprene material. The boot is 100% waterproof, temperature rated to -40 degrees, and provides maximum comfort and protection in any terrain. 

"Durability goes a long way in the field and it presents itself in these boots,” said Ron Reslow of BoneDriven TV. “The Pursuit Shadow protects my feet from the worst Mother Nature has to offer, while providing comfort and maneuverability.  Best boot on the market.”

Muck Boots’ new Pursuit Shadow hunting boot was recognized by two leading outdoor publications: Field & Stream and OUTSIDE Magazine. Field & Stream included the Pursuit Shadow in its annual Best of the Best: 41 Top New Products for This Hunting Season. Over 150 products were tested for this year’s list with the Pursuit Shadow ranking among only 41 fit to make the cut. The Pursuit Shadow was also the only hunting boot featured on the ‘Best of the Best’ list.  

OUTSIDE Magazine featured the Pursuit Shadow in its annual Winter Buyer’s Guide to the best gear for the winter sports season. The results of the magazine’s field tests of hundreds of products, make it a top resource for outdoor enthusiasts. Reviews are organized by sport and activity and only the best items on the market are featured in the guide. This is the second consecutive year that a Muck Boot product has made it into Winter Buyer’s Guide. 

New Fashion-Forward Styles

Taking inspiration of the stylish cities in Europe, the Muck Boots Diamond Collection includes fashion-forward styles with soft leather and on-trend silhouettes, but still features the unique neoprene material synonymous with any Muck Boot. 

The Como, a knee-high sleek leather boot on a stacked heel boasts style with substance, offering 100% waterproof protection and maximum comfort.  The Verona ankle boot features waterproof leather, a neoprene lining with a stylish trim and flair.  And finally, designed for country style anywhere, the Western is a 100% waterproof leather cowboy boot with the Muck Boot DNA built in for durability and comfort.