Media Contact


Bruce Eric Anderson

Home and Building Technologies

+1 (763) 954 5344

+1 (612) 990-0622 - Mobile

Email

Celebrate Outdoorsy Dads This Father's Day With the Latest Must-Have Footwear


If the fathers in your life have a love for the outdoors, surprise them this Father’s Day with must-have gear from The Original Muck Boot Company,  XTRATUF boots, Oliver by Honeywell and Honeywell’s Howard Leight. Whether they're hitting the trails, doing yard work, fishing, shooting or working in the shop, these Honeywell brands have them covered.

For the weekend warrior dad…
The Original Muck Boot Company Muckster II is perfect for the dad seeking comfort and function in an outdoor bootThe Original Muck Boot Company Muckster II is perfect for the dad seeking comfort and function in an outdoor boot. One of Muck Boots’ most versatile styles, these 100% waterproof shoes are available in both ankle and low height. The breathable air mesh lining makes them warm enough for cool, rainy days, but not too hot for when the sun comes out. Easy to slip on and kick off quickly, this boot also features a new sole and updated styling that gives this shoe more stability on wet surfaces. 

The Original Muck Boot Company offers free shipping and exchanges on all orders within the continental United States.

For the fishing, boats and cold-drinks-in-a-can dad…
The XTRATUF Performance Ankle Deck Boot is ideal for the father that fishes or the stylish dad that likes to kick back at the dockThe official XTRATUF Coolie has the same non-slip technology that’s featured in their iconic rubber boots for premium surface grip.The XTRATUF Performance Ankle Deck Boot is ideal for the father that fishes or the stylish dad that likes to kick back at the dock. This 100% waterproof boot features a lightweight design with a slip-resistant outsole, perfect for when hanging out on the deck during a family boat ride. An XpressCool™ lining keeps dad’s feet cool in warmer weather, making it his go-to summer boot. 

Dad will never lose a perfectly good beverage to slippery fingers or surfaces again! The official XTRATUF Coolie has the same non-slip technology that’s featured in their iconic rubber boots for premium surface grip, with a tread like that of the bottom of a fishing boot. Keeps your drink cool and exactly where you left it!

XTRATUF also offers free shipping and exchanges on all orders within the continental United States.
 
For the shooting enthusiast dad…
Give the dad who frequents the shooting range the gift of hearing protection with the Impact Sport Electronic Earmuffs from Honeywell’s Howard Leight. Give the dad who frequents the shooting range the gift of hearing protection with the Impact Sport Electronic Earmuffs from Honeywell’s Howard Leight. They protect hearing by automatically shutting off amplification when harmful sound levels are reached, blocking any continuous or impulsive noise over 82 dB. Available in several colors, including Mossy Oak® Break-Up Infinity® and Tactical® Black, the Impact Sport is the ideal hearing protection solution for those looking to blend in with their surroundings. Dad won’t have to worry about noise-induced hearing loss again and he can listen to his favorite tunes while on the range or the hunt by plugging any MP3 player or smartphone into the built-in AUX jack.  


For the Do-It-Yourselfer dad… 
With rich roots in mid-1800s Australia, Oliver Boots are known for their superior craftsmanship, designed as much for comfort and style as they are for safety and durability. For the dad who likes to take at-home projects into his own hands, Oliver boots’ soft and flexible underfoot will help diminish lower back, leg and foot fatigue while he’s hard at work. The Oliver 42 Series is a fully lined work boot with a soft toe and liquid-resistant leather for a classically rugged look. Equipped with All-Terrain TPU soling technology for a lightweight, shock absorbing midsole, Dad’s feet stay cushioned with every step.