How Turbo Works


You've heard the word "turbo" tossed around a lot, especially by performance car enthusiasts. But all you know is that it means an engine has more "oomph" to it than normal. But what exactly is going on underneath that hood? Let's open it up and take a look.

It's All About Better Combustion
Before you can truly appreciate what a turbocharger does for an engine, you need to understand the basics of internal combustion.

Internal combustion engines are "breathing" engines. That is to say, they draw in air and fuel for energy. This energy is realized as power when the air-fuel mixture is ignited. Afterward, the waste created by the combustion is expelled. All of this is typically accomplished in four strokes of the pistons.

What a turbocharger does is to make the air-fuel mixture more combustible by fitting more air into the engine's chambers which, in turn, creates more power and torque when the piston is forced downward by the resulting explosion. It accomplishes this task by condensing, or compressing, the air molecules so that the air the engine draws in is denser. Now, how it does that is the real story here.

A Tale Of Two Wheels
A turbocharger is basically an air pump. Hot exhaust gases leaving the engine after combustion are routed directly to the turbine wheel side of the turbocharger to make it rotate. That turbine wheel is connected by a shaft to a compressor wheel. As the turbine wheel spins faster and faster, it causes the compressor wheel to also spin quickly. The rotation of the compressor wheel pulls in ambient air and compresses it before pumping it into the engine's chambers.

As you may have guessed, the compressed air leaving the compressor wheel housing is very hot as a result of both compression and friction. So what's needed is a way to cool that air down before it enters the chambers. That's where a charge-air cooler (or "heat exchanger") comes in. It reduces the temperature of the compressed air so that it is denser when it enters the chamber (heat causes things to expand, as we all learned in science class). The charge-air cooler also helps to keep the temperature down in the combustion chamber. All together, the engine, turbocharger and charge-air cooler form what is known as a "charge-air system".

Some systems also include a tip turbine fan which draws air across the charge-air cooler to further reduce the temperature of the compressed air generated by the turbocharger.

Not As Easy As It Looks
The basic principal behind turbocharging is fairly simple, but a turbocharger is a very complex piece of machinery. Not only must the components within the turbocharger itself be precisely coordinated, but the turbocharger and the engine it services must also be exactly matched. If they're not, engine inefficiency and even damage can be the results. That's why it's important to follow correct installation, operating and preventative maintenance procedures.

Search