Check icon

Success

Your request has been successfully submitted.

Jiangsu Sailboat Petrochemicals Company Starts Honeywell UOP Methanol-to-Olefins Unit

DES PLAINES, Ill., Feb. 22, 2017 /PRNewswire/ -- Honeywell (NYSE: HON) announced that Jiangsu Sailboat Petrochemical Company, Ltd. started its UOP Advanced Methanol-to-Olefins (MTO) unit during a 10-day test to confirm successful operation. When the full unit goes on line, it will have an annual production capacity of 833,000 metric tons per year, making it the largest single-train MTO unit in the world.

 

Located in Lianyungang City in China's Jiangsu Province, the Sailboat facility will produce propylene for the production of acrylonitrile, which is used to make clothing and fabrics, and high-performance polymers used in automotive parts, hard hats and other hard plastic products. The plant also will produce ethylene for the production of ethylene vinyl acetate copolymers, which are used to make adhesives, foams, medical devices, photovoltaic cells, and other products, as well as C4 olefins for the production of butadiene, an ingredient in synthetic rubber.

 

"We expect China to invest more than $100 billion in coal-to-chemicals technology in the next five years," said Mike Millard, vice president and general manager of UOP's Process Technology and Equipment business. "With China's demand growth for propylene of 7 percent per year, ethylene demand growing nearly 6 percent, and butadiene at almost 4 percent, our Advanced MTO process provides an excellent solution to meet that demand."

 

Ethylene and propylene, the two most widely used components to make plastics in the world, have traditionally been derived from crude oil. For regions such as China that lack domestic sources of crude oil, the Advanced MTO Technology allows for the use of other more economical feedstocks such as coal and natural gas.

 

Jiangsu Sailboat chose the Advanced MTO process because it produces the highest yields of light olefins at the lowest cost of production, with the lowest catalyst consumption and the lowest operating cost. In addition, the unit is configured for production of C4 olefins, as well as ethylene and propylene.

 

Honeywell UOP's Advanced MTO process combines the UOP/Hydro MTO process and the Total/UOP Olefin Cracking Process to significantly increase yields and feedstock efficiency. The process converts methanol from coal and natural gas into ethylene and propylene. At the heart of the technology are UOP's proprietary catalysts, which make it possible to efficiently adjust the ratio of propylene and ethylene produced so operators can most effectively meet demand for those products.

 

Jiangsu Sailboat Petrochemical Co., Ltd. is a wholly-owned subsidiary company of Shenghong Holding Group, located in Xuwei new district Industrial Park, Lianyungang City, Jiangsu province. When fully completed, the 500-hectare facility will produce about 2.5 million tons of short-supply high-end petrochemical products annually.

 

Honeywell UOP (www.uop.com) is a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries. Honeywell UOP is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes Honeywell Process Solutions (www.honeywellprocess.com), a pioneer in automation control, instrumentation and services for the oil and gas, refining, petrochemical, chemical and other industries.

 

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

 

John Simley
Honeywell UOP
+1 (847) 612-1484  - Mobile