Check icon

Success

Your request has been successfully submitted.

More Connectivity for Your Home Devices

Honeywellnow.com_562x261_01_12_16

Honeywell’s Connected Thermostats Now Work With IFTTT And Samsung SmartThings

Consumers are increasingly looking for ways to connect their lives and homes. According to Honeywell’s Home Connectivity Survey, 90 percent of Americans have a desire to automate their homes in some way and are clamoring for new ways to do so. Thanks to new updates for a number of Honeywell connected thermostats managing home comfort has become even easier.

IFTTT Gives Homeowners More Home Comfort Flexibility

Honeywell has a new channel on the popular consumer app IFTTT that gives homeowners more options for remote control of their home comfort system. IFTTT, which stands for “If This, Then That,” is a web-based service that allows users to create chains of simple conditional statements, called recipes, to trigger actions from their connected devices. IFTTT recipes enable homeowners to automatically link to and manage their Honeywell Lyric™ or other Honeywell Wi-Fi Smart Thermostats using IFTTT’s simple, do-it-yourself “recipes.”

Users can create their own or utilize recipes that already exist on the IFTTT site. For example, if the temperature outside goes below 65° then set the temperature in the house to 72°.

With Honeywell Recipes on IFTTT, a connected thermostat is even more customizable to meet a homeowner’s needs.

Honeywell Lyric with Samsung SmartThings Can Make a Smarter Home

Honeywell has also joined together with the team at Samsung SmartThings to allow homeowners to connect and control a Honeywell Lyric™ (read news release) thermostat (first and second generation) through Samsung’s new SmartThings Hub and mobile app (available for iOS, Android, and Windows). The SmartThings Hub enables homeowners to manage and control connected devices in their home, such as smart locks, connected light bulbs and switches, speakers, and others.

Consumers who own a Lyric thermostat can now instantly adjust their home’s temperature through the hub and mobile app anytime or anywhere.Other Honeywell and SmartThings products, including Honeywell’s Wi-Fi Smart and Redlink thermostats, will be able to interact using the same secure cloud technology in the future.

How can I buy?

Pre-order or find a retailer for the new Lyric Round thermostat here.

The Samsung SmartThings Hub can be purchased at http://Shop.SmartThings.com ($99 U.S. MSRP) or from retailers including Amazon.com and Best Buy.

Learn more about which Honeywell connected thermostats are compatible with IFTTT, and the Samsung SmartThings Hub/SmartThings mobile app, by visiting http://yourhome.honeywell.com

Mark Hamel
Safety and Productivity Solutions
+1 (952) 334 4337  - Mobile