Check icon

Success

Your request has been successfully submitted.

Honeywell Makes Homes Smarter with the Lyric Wi-Fi Water Leak and Freeze Detector

The $79 sensor can alert homeowners to water leaks, mold, and freezing pipes quickly, whether you're at home or on the go.
You lock up the house, hop in the car and head out for the day and then that sinking feeling hits you. Did I leave the water running?

You're not always confident that you turned the faucet off before you left. The Honeywell Lyric Wi-Fi Water Leak and Freeze Detector can help you know if your home has a water situation happening.



According to the American Insurance Association and Insurance Services Office, damage caused by water, such as from a burst pipe or faulty appliance, can result in thousands of dollars of unanticipated repairs. In fact, water-related property damage exceeds $11 billion annually, with insurance claims averaging more than $7,000 per incident. Honeywell believes that your money could be better spent elsewhere &endash; think vacation! &endash; rather than cleaning up after leaky plumbing.

Place the Lyric Detector nearly anywhere in your home and it gives updates on humidity in the air and temperature and provides alerts if water is sensed by the four-foot cable or the contacts on the detector itself. If there's a problem, Lyric will tell you with an audible siren and an alert in the Lyric app. With push notifications, homeowners can set up an inner circle (from neighbors to friends and family) who also can also be notified when water is sensed.

Honeywell Makes Homes Smarter with the Lyric Wi-Fi Water Leak and Freeze Detector

No bigger than a hockey puck, the Lyric Detector easily sits under sinks, near appliances, close to sump pumps or any place that could have an issue with water. The included AA batteries ensure long battery life of up to three years and, once Lyric senses water, it can simply be reset to be used again. If you're worried about a larger room, such as a basement or laundry room, one Lyric Detector can have multiple cable sensors added together for up to 500 feet of continuous coverage.

So next time you hop in the car and you question whether you hit the faucet, remember that the Lyric detector has your back.

Water is great, but for those times when water isn't so great to your home, there's the Lyric Wi-Fi Water Leak and Freeze Detector to keep you in the know. The product is available today at The Home Depot or Best Buy for $79.

Visit http://lyric.honeywell.com or follow @Honeywell_Home for more on Honeywell's Lyric products for your connected home.


Bruce Anderson
Home and Building Technologies
+1 (612) 990-0622  - Mobile