Check icon

Success

Your request has been successfully submitted.

Honeywell's Spectra® Fiber Helps Make Prosthetic Limbs More Comfortable and Durable ÔøΩ Comfort Products Incorporates High-Performance Material into Knitted Products to Achieve Unmatched Strength and Resiliency

March 07, 2006

Honeywell's Spectra® Fiber Helps Make Prosthetic Limbs More Comfortable and Durable Comfort Products Incorporates High-Performance Material into Knitted Products to Achieve Unmatched Strength and Resiliency

Morristown, N.J., March 7, 2006: Honeywell (NYSE: HON) announced today its Spectra ® fiber is being used to make prosthetic limbs more comfortable and last longer.Comfort Products, the first U.S. provider of knitted orthotic and prosthetic products, uses Honeywell's high-performance material in its SpectraCarb™, a Spectra and carbon composite, for orthotic and prosthetic laminations, and in the custom-designed Spectra Sock which protects the inside of prosthetic limbs.Spectra is one of the world's strongest and lightest fibers. It has the highest strength-to-weight ratio of any synthetic fiber, including nylon, polyester and aramid. Pound-for-pound, Spectra fiber is 10 times stronger than steel, yet is soft enough to be used in clothing, protective gear and other products designed to be worn for prolonged periods."Spectra fiber's strength has made it a material of choice for military armor, protective gear and high-performance ropes," said Elizabeth Parrish, global marketing manager for Honeywell's Advanced Fibers and Composites business. "These same characteristics make it ideal for prosthetics, where improvements in strength, resiliency and weight can make all the difference."Traditionally, prosthetic limb manufacturers used carbon to add strength. However, its rigidity often created razor-sharp edges that could damage suspension sleeves an aid that partially covers the prosthesis and the patient's exposed skin and the prosthetic's external casing. These edges can cause discomfort for users.More than 1.2 million people in the U.S. are missing extremities, according to the industry's leading trade association.Comfort Products uses SpectraCarb to create strong, flexible sockets that fit around residual limbs and allow prosthetics to properly attach and fit. Older, carbon-based sockets were too rigid to allow internal adjustments after the initial lamination, and a new socket would have to be created if it did not properly fit the amputee. SpectraCarb allows professionals to shape and adjust the socket for a better fit. SpectraCarb also provides a more flexible, comfortable socket for the user, and a more cost-effective product for the manufacturer.Spectra Socks protect prosthetic limbs from damage caused by sharp internal carbon structures. The sock extends the life of the prosthetic limb, saving amputees and medical companies from the aggravation and economic cost of frequent replacements. In addition, the Spectra Sock eliminates squeaking noises that often result from the constant motion of the internal carbon structures during use.Comfort Products provides Spectra-based products to Windy City Fabricators, a brace and artificial limb manufacturer."Our Spectra fiber-based products provide unmatched resiliency, so the people wearing them have fewer visits to the doctor resulting from performance problems or discomfort," said Peter Panuncialman, president of Windy City Fabricators. "The SpectraCarb products offer great comfort because they're more flexible than carbon-only products.""By using Spectra fiber, we've been able to deliver on our vision of providing individuals with prosthetic and orthotic products that are more comfortable and durable," said Michael Burton, director of sales and marketing at Comfort Products.Honeywell International is a $28 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, Chicago and Pacific Stock Exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com.Honeywell Specialty Materials, based in Morristown, N.J., is a global leader in providing customers with high-performance specialty materials, including fluorine products; specialty films and additives; advanced fibers and composites; intermediates; specialty chemicals; electronic materials and chemicals; and technologies and materials for petroleum refining.This report contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.