Check icon

Success

Your request has been successfully submitted.

Popular Science Names Hurricane-Resistant Curtain Containing Honeywell Spectra® Fiber ÔøΩBest of What's New'

November 18, 2008

Popular Science Names Hurricane-Resistant Curtain Containing Honeywell Spectra® Fiber Best of What's New'

Protective curtains take top honors in the home technology categoryMORRIS TOWNSHIP, N.J., Nov. 18, 2008: Honeywell (NYSE: HON)announced today that Popular Science magazine has awarded a 2008 Best of What's New Grand Award to hurricane-resistant curtains containing Honeywell's high-strength Spectra ® fiber. The curtains were named the top innovation in home technology.Honeywell's Spectra fiber, commonly used in bullet-resistant body armor,enables the Storm-A-Rest ™ curtains to protect windows and doors during hurricanes. Because it uses Spectra fiber, the roll-down curtains can withstand 155 mph winds and impact from large wind-borne projectiles. They are manufactured by North Carolina-based JHRG, LLC."We are honored that Popular Science has recognized the role our high-strength Spectra fiber is playing in hurricane protection," said Joe Gelo, global business director for Honeywell's Advanced Fibers and Composites business. "It is further evidence that Spectra fiber can help end-use products perform in the harshest of conditions."Storm-A-Rest curtains are approved under Florida's building code for Wind Zone 4, which includes the area within one mile of the state's nearly 1,200-mile coastline. It is estimated that 7.3 million homes are within the hurricane zone.Homeowners can easily install the curtains using standard fasteners without special tools. They can be fastened to wood, brick or concrete surfaces. The curtains are available in more than 350 Sunbrella ®-brand accent patterns and come with a five-year warranty. Unlike alternatives like plywood and corrugated aluminum panels, Storm-A-Rest panels are easy to install,maintain and store. Because the curtain incorporates Honeywell's Spectra fiber,they are extremely lightweight, weighing less than two ounces per square foot about 75 percent less than corrugated aluminum panels."For 21 years, Popular Science's Best of What's New awards honor the innovations that make a positive impact on life today and change our view of the future," said Mark Jannot, editor-in-chief of Popular Science."PopSci's editors evaluate thousands of products each year to develop this thoughtful list; there's no higher accolade Popular Science can give."Pound for pound, Spectra fiber is 15 times stronger than steel. It is made from ultra-high molecular weight polyethylene using a patented gel-spinning process.The fiber exhibits high resistance to chemicals, water, and ultraviolet light.It has excellent vibration damping, flex fatigue and internal fiber-friction characteristics. It also has up to 60 percent greater specific strength than aramid fiber.Other industrial applications for Spectra fiber include security netting, rope and cordage and fishing line, as well as industrial slings used to lift heavy requipment and materials for offshore oil and gas construction.Honeywell maintains an active Spectra fiber and ballistic material research and development program aimed to meet increased demand for its high performance materials. For more information about Spectra fiber, visit http://www.honeywell.com/spectra.Founded in 1872, Popular Science is the world's largest science and technology magazine, with a circulation of 1.3 million and 6.8 million monthly readers.Each month, Popular Science reports on the intersection of science and everyday life, with an eye toward what's new and why it matters. Popular Science is published by Bonnier Active Media, a subsidiary of Bonnier Corporation.Storm-A-Rest is a trademark of JHRG, LLCSunbrella is a registered trademark of Glen Raven Inc.Honeywell Specialty Materials, based in Morristown, N.J., is a $4.9 billion,global leader in providing customers with high-performance specialty materials,including fluorine products; specialty films and additives; advanced fibers and composites; intermediates; specialty chemicals; electronic materials and chemicals; and technologies and materials for petroleum refining.Honeywell International is a $38 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; specialty chemicals; fibers; and electronic and advanced materials. Based in Morris Township, NJ, Honeywell's shares are traded on the New York, London, Chicago and Pacific Stock Exchanges. It is a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com.This report contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occurIn the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.