Check icon

Success

Your request has been successfully submitted.

HONEYWELL INTRODUCES THE FIRST UNIVERSAL DIGITAL OIL PRIMARY WITH A BUILT-IN DIAGNOSTIC DISPLAY

MINNEAPOLIS, Aug. 18, 2010 Honeywell (NYSE: HON) today introduced the R7284U Universal Digital Oil Primary control with built-in diagnostic display, which allows an oil service technician to determine the root cause of a lockout as well as access every setting and diagnostic feature of the control without having to use additional tools.The R7284U provides detailed historical information about the control from daily performance to system failure. It also offers complete universality by allowing for field configuration of the lockout time and delay on and off times. The easy-to-read screen is also programmable in English, Spanish and French."The display lets oil dealers know where to look for the problem and provides actionable diagnostics that save the oil dealer installation time, reduce call-backs and help make them more money," said Rich Simons, director of product marketing, Honeywell Residential Combustion Control. "In the event of an oil burner component's failure, the display will tell the oil dealer which component on the oil burner is defective."The Universal Digital Oil Primary is compatible with nearly all oil-fired appliances and can fully integrate into any EnviraCOM™ communications system, allowing for both local and remote diagnostics on equipment with a three-wire connection.For more information on Honeywell's Universal Digital Oil Primary, visit http://www.forwardthinking.honeywell.com/R7284.Honeywell Universal Digital Oil PrimaryHoneywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Environmental & Combustion Control is part of the Honeywell Automation and Control Solutions business group, providing integrated product solutions in heating and heating processes, ventilation, cooling and refrigeration, air filtration, zoning, humidification, air conditioning, water controls and processes, electrical devices and systems, lighting control, buildings controls, switches, sensors and controllers. ECC's technologies are found in more than 150 million homes, 10 million buildings, and a multitude of manufacturing plants around the world.This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.