Check icon

Success

Your request has been successfully submitted.

HONEYWELL INTRODUCES FLEXIBLE, EFFICIENT EVAPORATIVE HUMIDIFIERS TO IMPROVE PROFITABILITY OF CONTRACTORS

MINNEAPOLIS, Sept. 23, 2010 Honeywell (NYSE: HON) today introduced TrueEASE, a complete family of evaporative humidifiers that reduce contractor installation time and help improve the profitability of a contractor's business. The advanced design and patent-pending features of the TrueEASE™ whole-house humidification system offers maximum versatility and efficiency all significant features for installers and homeowners alike."With an emphasis on innovative design, operation, installation and maintenance, TrueEASE addresses the needs of contractors and homeowners alike," said John Tyhacz, vice president and general manger for Honeywell's Home Comfort and Energy Systems business.TrueEASE is 20 percent faster to install than other evaporative humidifiers. The patent-pending interchangeable bypass eliminates the need to disassemble and rebuild the humidifier if the bypass direction needs to be changed. The mounting screws located around the perimeter of the humidifier make single-step installation possible rather than mounting a separate frame assembly.TrueEASE cycles water and air through the system only when humidity is needed; using up to 50% less water. It also helps save energy by eliminating the constant cycling of air.Push terminals and an integrated control board reduce cost and time spent on separate relays typically required to deliver additional humidity. A simple flip of the DIP switch sets advanced humidification options.Additional features of TrueEASE include:Quick Connect Plumbing allows contractors to connect the plumbing in a single-step by attaching the hose to the quick connect gasket.PerfectFLO™ Water Distribution Tray distributes water evenly across the padHoneywell TrueEASE Evaporative HumidifiersCommon-Sense Interface indicates when the system is humidifying, when it's time to replace the pad and when the humidifier needs serviceAgION® Humidifier Pad features an anti-microbial coating to inhibit the growth of molds, bacteria, fungus and algae on the pad.Customized Label Program generates lasting customer relationships through product customizationFor more information on Honeywell's TrueEASE Humidification Systems or other indoor air quality products or controls, please visit www.forwardthinking.honeywell.com.Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Environmental & Combustion Control is part of the Honeywell Automation and Control Solutions business group, providing integrated product solutions in heating and heating processes, ventilation, cooling and refrigeration, air filtration, zoning, humidification, air conditioning, water controls and processes, electrical devices and systems, lighting control, buildings controls, switches, sensors and controllers. ECC's technologies are found in more than 150 million homes, 10 million buildings, and a multitude of manufacturing plants around the world.This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.TrueEASE™ is a trademark of Honeywell International Inc.