MAKS, MOSCOW, Aug. 27, 2013 – Honeywell Aerospace (NYSE: HON) has been selected by Russia’s Siberian Aeronautical Research Institute (SibNIA) to supply an expected 300 TPE331-12UAN turboprop engines as part of a major upgrade offering for Russia’s Antonov An-2 fleets, with an option for additional orders. Starting in late 2013, Honeywell will supply the engines and aftermarket support to improve the operational capabilities and efficiency of the An-2.Honeywell’s TPE331-12UAN engine is a derivative of the proven TPE331-12UHR that powers the Jetstream 32 and Metro 23, and will provide 1,100 takeoff shaft horsepower (SHP) for the An-2. SibNIA selected the engine because of its performance, fuel efficiency, proven reliability and demonstrated ability to support operations in remote and challenging environments.The An-2 is a versatile utility biplane with unique capabilities including remarkable short takeoff and landing performance, low-speed handling, large payload capacity and the ability to operate out of unprepared fields.SibNIA’s overhaul of the An-2 will bring some of the industry’s latest engineering to the platform and comes at a time when the Russian government is increasing its focus on aerospace and, in particular, aviation infrastructure in remote areas. Government and private operators upgrading their An-2 fleets with SibNIA will benefit from the TPE331’s versatile and robust design to complete a wide range of missions including local air transport, firefighting, aerial spraying, medevac and training.Honeywell and SibNIA are also considering additional opportunities for future collaboration on the An-2 program. These could include avionics, with both manufacturers exploring concepts for upgrading the An-2 cockpit using the extensive capabilities of Honeywell’s avionics product line, as well as the potential for localized production of the TPE331-12UAN. SibNIA will be the focal point for TPE331 engine support in Russia for the An-2, building gradually from line maintenance to overhaul as dictated by aircraft fleet utilization and operational needs.
TPE331 benefits include:• Lower weight and compact installation to reduce fuel burn• Fastest turboprop response rate in the industry• Proven in utility operations in diverse environments• Extended maintenance scheduling and proven reliability ideal for remote operations• Operates on most common jet fuels including TS1, approved for this programSince its market introduction in the 1960s, Honeywell’s TPE331 has been at the forefront of turboprop propulsion, and includes 18 models and more than 100 configurations across the product family.
Supporting Quotes
Victor Valente, Vice President, Business and General Aviation EMEAI, Honeywell Aerospace•
“Our TPE331’s performance and response rate are integral to the remarkable performance improvement offered by the re-engined An-2. The TPE331’s reliability record is a powerful enabler for the diverse and remote operations that are typical of the An-2 fleet, and the engine is a great example of how Honeywell can bring new operational capabilities and life-cycle extension to older, yet perfectly capable, aircraft.”
Vladimir Barsuk, Director, SibNIA•
“For the An-2 re-engine element we needed an engine partner that could provide a fuel-efficient, easy-to-maintain, high-performing and robust propulsion system on time and without unexpected challenges or delays. These requirements have been met by Honeywell as we move forward with the aircraft overhaul program swiftly and without surprises. The combination of its proven record as a leading aerospace supplier and product support capabilities makes Honeywell the perfect partner for the An-2 re-engine program.”Honeywell is showcasing its commercial, business, helicopter and general aviation capabilities at MAKS 2013, in Zhukovsky, Moscow, from Aug. 27–Sept. 1, at Booth #B36 in the U.S. pavilion. Also at the show, SibNIA will be showing a Yakovlev YAK-40 regional jet powered by Honeywell TFE731 engines.
Supporting Resources• About Honeywell at
MAKS 2013• About Honeywell’s
Business Aviation products and services• Read more about
Honeywell Aerospace• Follow
@Honeywell_Aero on Twitter• Subscribe to Honeywell’s
Corporate RSS feed
About Honeywell RussiaSince the 1930s, Honeywell has provided technologies to Russia that improve safety, security, operational efficiency and profitability across many sectors, from residential to commercial and industrial and including critical infrastructures such as airports, hospitals, sports stadiums, and public buildings and facilities. It also has a long history of development in Russia’s oil and gas industries, including the modernization of refineries.Honeywell collaborates with many Russian universities, including Moscow Institute of Physics and Technology, Gubkin Russian State Oil and Gas University, Saint-Petersburg Technological University and Ufa State Oil Technical University, as well as with entities such as Rusfilter, Boroskov Institute, BARS, Lukoil Inform, the Russian design institutes and others. More than 650 professionals support Honeywell’s operations in Russia, covering all four strategic business units: Aerospace, Automation and Control Solutions, Performance Materials and Technologies, and Transportation Systems.
About Honeywell AerospaceThousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. For more information, visit
http://aerospace.honeywell.com or follow us at
@honeywell_aero on Twitter.Honeywell (
www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit
www.honeywellnow.com.Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2013 Honeywell.This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.