Check icon

Success

Your request has been successfully submitted.

Honeywell Solstice™ Liquid Blowing Agent Receives Voc-Exempt Status From U.S. Epa

September 25, 2013

Honeywell Solstice™ Liquid Blowing Agent Receives Voc-Exempt Status From U.S. Epa

New, environmentally preferable technology for foam insulation allows manufacturers to meet federal regulationsMORRIS TOWNSHIP, N.J., Sept. 25, 2013 &emdash; Honeywell (NYSE: HON) announced today that the U.S. Environmental Protection Agency (EPA) has added Solstice™ Liquid Blowing Agent, also known as 1233zd, to the list of materials exempted from volatile organic compound (VOC) regulations.The classification will help manufacturers develop products that meet federal VOC regulations. The exemption further demonstrates the environmental benefits of Solstice LBA, which has a global warming potential (GWP) of less than 1 (lower than carbon dioxide), significantly lower than the GWP of traditional hydrofluorocarbon (HFC) blowing agents, and an order of magnitude lower than the GWPs of many hydrocarbons.Blowing agents allow closed-cell foam insulation to expand and provide the majority of the foam's excellent insulating properties. They are used by refrigerator manufacturers, spray foam insulation formulators and insulated panel manufacturers to provide superior insulating properties to a variety of end-use products including appliances, roofs and walls."Customers need a blowing agent that offers both outstanding thermal insulation performance and superior environmental properties. Solstice LBA offers just that &emdash; it is VOC-exempt, has an ultra-low GWP, and is nonflammable," said Rajiv Banavali, chief technology officer for Honeywell Fluorine Products.Solstice LBA is a cost-effective, energy-efficient and environmentally preferable alternative to high-global-warming-potential HFC blowing agents.VOCs are organic compounds that break down quickly in the lower atmosphere and participate in chemical reactions that ultimately create tropospheric (ground-level) ozone, which is an irritant and a major component of smog. The EPA provided the VOC exemption for Solstice LBA based on the material's low photochemical reactivity and negligible contribution to the generation of ground-level ozone.In addition to Solstice Liquid Blowing Agent, Honeywell's family of Solstice-branded products includes stationary and mobile refrigerants, gaseous blowing agents, propellants and solvents based on Honeywell's new hydrofluoro-olefin technology that helps customers lower their carbon footprint without sacrificing end-product performance. The products have been developed and are being commercialized by Honeywell's Fluorine Products business, a leader in the manufacture and supply of non-ozone-depleting blowing agents for energy-efficient foam insulation.For more information, please visit www.honeywell-blowing agents.com.Honeywell Performance Materials and Technologies is a global leader in developing and manufacturing advanced materials and process technologies. These materials and technologies are used by people every day in a wide range of industries and applications, from petroleum refining to environmentally friendlier refrigerants to bullet-resistant vests. Our advanced materials are critical in the manufacture of products ranging from nylon to computer chips to pharmaceutical packaging. Process technologies developed by our UOP business form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel and petrochemicals. UOP is now pioneering technology to produce real fuels from renewable energy sources.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
# # #
Contact:Jeannine Sohayda973-455-2706 jeannine.sohayda@honeywell.com