Check icon

Success

Your request has been successfully submitted.

RAE Systems Launches Fixed Gas Detection System For Enhanced Industrial Safety

Company's New Line of Economical, Highly Scalable Fixed Systems Gas Detection Solutions Provide Enhanced Plant-Wide Safety San Jose, Calif. – Oct. 1, 2013 – RAE Systems Inc., the leader in connected gas and radiation detection solutions, today introduced a new line of advanced, fixed-systems gas detection products that elevate safety for workers and responders operating in hazardous industrial environments. These monitors include the RAEGuard 2 photoionization detector (PID) for continuous volatile organic compound (VOC) monitoring, and RAEAlert toxic and flammable fixed gas detectors and FMC system level controllers. RAEGuard 2 PID - Fixed Detector for VOC monitoring in hazardous and non-hazardous area locations.Workers at industrial facilities and oil and gas refineries face the constant threat of exposure to toxic and combustible gases at potentially lethal levels. Safety officers need solutions in place that allow for continuous gas monitoring to enhance plant-wide safety and mitigate risk via an advanced system approach. RAEGuard 2 PID Fixed Detector The new RAEGuard 2 PID offers continuous VOC monitoring in hazardous and non-hazardous area locations, with fast response times and a high level of accuracy of readings. Its proprietary third-generation PID sensor technology allows a wide range of resolutions that can be as low as 10 ppb and as high as 1,000 ppm. Maintenance costs have been significantly reduced due to an easily removable / replaceable sensor module. The sensor and lamp can be removed without tools and serviced in any location, which greatly simplifies calibration and maintenance requirements.The RAEGuard 2 PID’s explosion-proof stainless-steel enclosure makes it suitable for outdoor applications in hazardous Class I, Division 1 (ATEX Zone 1) environments. RAEAlert Fixed DetectorsThe RAEAlert line of fixed gas detectors delivers an economical solution for continuous air monitoring in hazardous environments. This highly scalable solution offers up to nine different sensor options, optional LCD displays, optional relays, and optional infrared remote controllers. The RAEAlert line provides safety officers with maximum flexibility in system design by including sensor options for flammable, oxygen and various toxic gases.The explosion-proof design uses cast-aluminum housing and is certified for use in Class I, Division 1 (ATEX Zone1) environments. All RAEAlert detectors communicate via 4-20mA analog or RS485 digital signal protocols, and non-intrusive calibration and maintenance are performed with an intrinsically safe infrared (IR) remote. Fixed Systems Controllers: FMC 2, 4, 16 and 64RAE Systems is also introducing four new fixed systems controllers that are compatible with the RAEGuard 2 PID and RAEAlert line of fixed detectors. The FMC-2, FMC-4, FMC-16, and FMC-64 controllers are highly configurable and customizable, and provide simultaneous display and alarm functions for up to 64 sensor transmitters. These easy-to-configure, user-friendly controllers are ideal for centralizing display and alarm functions in critical multi-point monitoring applications.All of the controllers offer configurations that are certified for use in Class I, Division 2 hazardous environments. The FMC-64 offers advanced network capabilities and IP-addressable remote log-in for simultaneous viewing and sharing of time-critical threat data across geographically dispersed teams.“Industrial organizations cannot afford to risk worker, responder or public safety when a critical situation arises,” stated Thomas Negre, vice president of products and marketing for RAE Systems. “The new RAEGuard 2 PID, RAEAlert fixed detectors and FMC controllers give safety officers access to the most complete, comprehensive solution for continuous monitoring throughout a facility. RAE Systems’ new monitors and controllers provide a cost-effective and highly customizable system approach for enhancing plant-wide safety and mitigating risk.” AvailabilityThe RAEGuard 2 PID is available now in all regions. The RAEAlert will be available beginning in October 2013 in the EU and other regions that accept IECEx and ATEX approvals. RAEAlert will be available by the end of the year in North America and other regions that accept UL and CSA approvals. The FMC controllers will be available beginning in October 2013 in North America and will be available by the end of the year in regions that require CE approvals. Customers interested in obtaining more information or purchasing the new RAEGuard 2 PID, RAEAlert fixed detectors and FMC controllers should contact their RAE Systems Distributor or RAE Systems regional sales manager. About RAE Systems RAE Systems innovates, designs and manufacturers gas sensors and radiation detectors. The company offers a full line of fixed and portable gas detection solutions, including handheld and personal chemical, compound and radiation detection instruments. RAE Systems’ real-time safety and detection systems have been deployed by organizations in the oil and gas, fire and HazMat, industrial safety, national security and environmental markets, helping save lives and maintain safety in 120 countries. The company’s industry-leading gas sensors and radiation detection solutions are widely recognized for their performance and reliability. Learn more at raesystems.com.On June 4, 2013, Honeywell (NYSE: HON) completed its acquisition of RAE Systems Inc. The company will be integrated into Honeywell Analytics, part of Honeywell Life Safety (HLS) within Honeywell Automation and Control Solutions (ACS). Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.