Check icon

Success

Your request has been successfully submitted.

AT&T and Honeywell to Redefine the Air Travel Experience with World-Class, High-Speed Wireless Internet

New 4G LTE-based service to meet passengers’ online demand and help make the “Connected Aircraft” a reality

PHOENIX, Ariz., April 28, 2014 — Honeywell Aerospace (NYSE: HON) will be the exclusive hardware provider of domestic air-to-ground communication for AT&T’s planned in-flight connectivity services, which will bring faster Wi-Fi to passengers on commercial airlines and business jets. With the new 4G LTE service, passengers will experience speeds that are a significant improvement from today’s air-to-ground speeds. The service is anticipated to become available as early as the end of 2015.
Under terms of an agreement in principle with AT&T, Honeywell will build and deliver on an exclusive basis aircraft hardware needed to connect AT&T’s planned air-to-ground system in the U.S. With the new service, passengers will be able to enjoy 4G LTE’s fast and dependable connections to watch video, text with family and friends, and access quicker speeds to surf the internet. This system is being developed so that it can integrate with Honeywell’s GX and L-Band satellite systems allowing true regional and potentially global connectivity for passengers, crew and operations personnel
“Honeywell has established itself not only as a technology development leader but as the company that fully understands consumers’ desires to stay connected whether at home, in the office or car, and in-flight through the Connected Aircraft,” said Tim Mahoney, president and CEO of Honeywell Aerospace. “AT&T’s industry leadership in consumer communications, coupled with Honeywell’s expertise in aviation, satellite communications and now the connected home and the connected aircraft is the perfect match to meet the growing connectivity requirements in a rising market.”
About Honeywell’s Path to the Connected Aircraft
Through the acquisition of EMS Technologies in 2011, Honeywell has added new and complementary technologies to its air-to-ground and satellite communications portfolio. That strategic expansion coupled with Honeywell’s existing satellite communications expertise led to the company winning hardware and business aviation service contracts for Inmarsat’s GX Aviation satellite constellation, set to be fully operational in 2015. Today, the company is expanding its air-to-ground connectivity solutions through a growing relationship with AT&T that includes plans to launch a new high-speed 4G LTE based in-flight Wi-Fi service for passengers, crews and operation personnel.
 

Thousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. 

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.