Check icon

Success

Your request has been successfully submitted.

MILLER AIRCORE NAMED "NEW PRODUCT OF THE YEAR"BY OH&S MAGAZINE

SMITHFIELD, RHODE ISLAND, Sept. 16, 2014 The Miller AirCore™ family of harnesses has been named "New Product of the Year" in the fall protection product category in Occupational Health & Safety (OH&S) magazine's sixth annual new product competition.A total of four honors went to Honeywell safety products the most awarded in the contest this year to a single personal protective equipment (PPE) manufacturer. The awards represent the continuing dedication of Honeywell Safety Products to introducing innovations that keep workers safe and support workplace cultures of safety around the world. The OH&S contest attracted more than 60 products in 22 award categories, with an independent panel of three highly qualified judges choosing the winners.The four Honeywell "New Products of the Year" are:
  • The award winning Miller AirCore™ harnesses are lightweight, full-body harnesses designed with breathable, open-core padding technology to improve air flow and keep workers drier and cooler. Now available in a variety of configurations, these innovative harnesses provide superior comfort and safety for a range of industries, including Construction, General Industry, Utilities, Oil & Gas, and Wind Energy. Visit: http://hwll.co/nwkh.
  • Uvex Livewire™ sealed eyewear, which deliver the fit, performance and protection required in extreme environments, to protect workers against intense wind, sun, dirt, dust and debris, as well as high heat and humidity. Based on extensive research and fittesting, the Uvex Livewire precision-engineered frame ensures a superior, gap-free fit that seals out debris, while the high-performance Uvextreme® Plus lens coating delivers 10 times longer anti-fog protection and two times better scratch resistance than competitive anti-fog coated products. Visit: http://hwll.co/vrqz.
  • The new North® CF7000 Series Abrasive Blast Respirator, developed to solve the tough environmental and physical challenges workers encounter during abrasive blasting operations. The Respirator features an innovative, lightweight design with 160? panoramic range of vision and a distortion-free lens replacement system that improves worker safety and productivity. The CF7000 Series is NIOSH-approved as a Continuous Flow Supplied Air and Air Purifying Respirator (when used with North P100 filters). Visit: http://hwll.co/7czb.
  • Oliver Footwear, which offers work boots that combine stylish leather craftsmanship with superior protection from harsh chemicals, temperatures, slippery conditions, and unexpected contact with abrasive surfaces or heavy machinery. Technologically advanced features like PORON® XRD® metatarsal guards, wider profile steel toe caps, PORON inserts and NONOlite footbed make Oliver footwear one of the most comfortable safety work boot lines in the marketplace. Visit: http://hwll.co/l94s.
About Honeywell Safety ProductsHoneywell Safety Products (HSP), a global manufacturer of leading personal protective equipment (PPE) and provider of safety solutions, helps company employees make safer decisions on their own and build an enduring culture of safety. With world class brands such as Honeywell®, Uvex®, North®, Howard Leight®, Miller®, Fibre-Metal® and Servus®, HSP offers a full range of quality PPE, including: protective clothing; fall and hearing protection products; solutions that protect hands, head, feet, eyes and face; along with respiratory, welding, first-aid, lockout/tagout and traffic safety equipment. Lead them to safety visit www.honeywellsafety.com/culture to learn more.bout HoneywellHoneywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.