Check icon

Success

Your request has been successfully submitted.

Honeywell, Boeing Demonstrate First GPS-Based Category III Precision Landing Ability

Demonstrated on the Boeing ecoDemonstrator 787, Honeywell’s SmartPath and upgraded receivers pave the way for increased air capacity with improved on-time arrivals and takeoffs PHOENIX, June 10, 2015 – In an industry first, Honeywell Aerospace ( NYSE: HON) and Boeing demonstrated how an airplane can use Honeywell’s next-generation, precision navigation and landing technology to perform safe and successful airport runway approaches and landings in weather conditions with a ceiling allowing no decision height and a minimum runway visual range of as low as 150 feet or Category III.Honeywell and Boeing have successfully demonstrated how airports that experience frequent visibility issues such as low cloud cover or fog will be able to implement future Honeywell SmartPath versions that enable these Category III (CAT III) landings to reduce delays and diversions due to bad weather.“Today’s airspace is crowded and on track to be even more crowded in the next 10 years. Airlines and airports need a more efficient and modern system to handle the influx of planes during approach and landing, specifically when the weather gets bad and pilots are operating in CAT III conditions,” said Bob Smith, chief technology officer, Honeywell Aerospace. “Honeywell has invented and tested a precision landing system that will not only alleviate crowded approaches and landings at airports, but will also give pilots the ability to land when they can’t see the runway, keeping airports and flights running efficiently.”Using Honeywell’s SmartPath Ground-Based Augmentation System (GBAS), Boeing used its ecoDemonstrator 787, a flight test airplane that in 2014 served to assess more than 25 technologies to reduce aviation’s environmental footprint, to complete 12 CAT III approaches and landings at Boeing’s test facility in Moses Lake, Washington. The aircraft also used Honeywell’s Integrated Navigation Receiver (INR), a navigation receiver that integrates the instrument landing signal, VHF omnidirectional range marker beacon and GBAS landing system navigation signals into a compact and more efficient unit.“Using the capability of today’s aircraft and the precision of global-based navigation, airlines can now land in very low-visibility weather conditions,” said Jeanne Yu, director of Environmental Performance at Boeing Commercial Airplanes. “This improves operational efficiency, saves fuel and reduces carbon dioxide emissions.”To successfully complete the CAT III approaches, which involve performing landings automatically in difficult conditions including fog, clouds, rain or other weather phenomena, Honeywell upgraded the software of the 787 INR and SLS-4000 SmartPath GBAS to support the additional CAT III monitoring and availability requirements. Honeywell Precision NavigationHoneywell has provided next-generation navigation technology to airports and airlines for decades. Its SmartPath precision landing system provides airports and airlines with a cost-effective solution that enables increased airport capacity, decreased air traffic noise, reduced weather-related delays and reduced operating costs. SmartPath accomplishes this by using signals from the Global Positioning System to provide aircraft operators with a very precise, digital navigation signal for precision approaches and landings.SmartPath is currently being used with revenue-generating flights and was designed to be upgradable to support CAT III landings and approaches.As well, Honeywell is continuing to implement these new technologies into its airborne navigation products such as the Integrated Multi-Mode Receiver, with the ability to upgrade via software updates.
Supporting Resources- Read more about SmartPath- Read more about Honeywell Aerospace and on the Follow The Aero blog- Like Honeywell Aerospace on Facebook- Follow @Honeywell_Aero on Twitter- Subscribe to Honeywell’s Corporate RSS feedHoneywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel-efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics, and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2015 Honeywell. For further informationGwennie Cheung Honeywell Aerospace +1 (646) 589-1741 gwennie.cheung@honeywell.com Honeywell Aerospace Media Center