Check icon

Success

Your request has been successfully submitted.

Honeywell Announces New PTM6000 Advanced Thermal Management Material For Semiconductor Manufacturing Applications

October 01, 2015

Honeywell Announces New Ptm6000 Advanced Thermal Management Material For Semiconductor Manufacturing Applications

Contact:Lance Chapman408-962-2098lance.chapman@honeywell.com Technology helps devices stay cool, perform betterMORRIS PLAINS, N.J., Oct. 1, 2015 &emdash; Honeywell (NYSE: HON) Electronic Materials announced the availability of its new Honeywell PTM6000 Phase Change Material (PCM). PTM6000 is the latest in Honeywell's line of Thermal Interface Materials (TIMs) which are used to transfer and dissipate heat from advanced semiconductor devices."More and more, device manufacturers need thermal management materials that provide high-end performance and long lasting reliability," said Olivier Biebuyck, vice president and general manager of Honeywell Electronic Materials. "Prior thermal management options often forced manufacturers to choose between immediate performance needs and overall reliability. PTM6000 has been designed and tested to meet both of these needs."Honeywell is a recognized leader in developing thermal management solutions. Honeywell's proven PTM and PCM series of thermal management materials are based on sophisticated phase-change chemistry and advanced filler technology that was developed specifically for high-performing electronic devices.TIMs technology from Honeywell transfers thermal energy from the chip to the heat sink or spreader, where it is dissipated into the surrounding environment. This functionality keeps the chip cool while allowing the heat sink module to perform optimally.Honeywell's unique, proprietary and patented formulations provide long-lasting chemical and mechanical stability, enabling consistently higher thermal performance compared with alternative thermal interface materials that break down or dry out.Honeywell offers an extensive family of Phase Change Materials (PCM) which meets the differing needs of multiple applications. PTM6000 was specifically designed for applications like automotive, high-power and high-performance servers which require long-lasting reliability and extreme thermal stability.The performance and reliability of PTM6000 has been proven through the industry's most widely accepted accelerated aging tests including: extended baking at 150 degrees Celsius (more than 300 degrees Fahrenheit) for 3000 hours; thermal cycling from -55 to 125 degrees Celsius (-67 to 257 degrees Fahrenheit); and the Highly Accelerated Stress Test (HAST). Honeywell PTM6000 passes these tests while meeting aggressive thermal needs such as thin bond line capability, low thermal impedance (<0.16&emdash;Ccm2/W @ 2mil) and long-term reliability.Honeywell Electronic Materials, part of Honeywell Performance Materials and Technologies, supplies microelectronic polymers, electronic chemicals, and other advanced materials along with an extensive set of product offerings under its metals business segment, including physical vapor deposition (PVD) targets and coil sets, precious metal thermocouples, and low alpha emissivity plating anodes and advanced heat spreader materials used during back-end packaging processes for thermal management and electrical interconnect.For more information about Honeywell's thermal management materials, or to contact a Honeywell representative, visit www.electronicmaterials.com.Honeywell Performance Materials and Technologies (PMT) is a global leader in developing advanced materials, process technologies and automation solutions. PMT's Advanced Materials businesses manufacture a wide variety of high-performance products, including environmentally friendlier refrigerants and materials used to manufacture end products such as bullet-resistant armor, nylon, computer chips and pharmaceutical packaging. Process technologies developed by PMT's UOP business ( www.uop.com) form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel, petrochemicals and renewable fuels. PMT's Process Solutions business ( www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas, refining, pulp and paper, industrial power generation, chemicals and petrochemicals, biofuels, life sciences, and metals, minerals and mining industries.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.