Check icon

Success

Your request has been successfully submitted.

U.S. Army Awards Honeywell $30 Million to Help Keep Chinooks Mission-Ready and Reliable

Maintenance contract provides engine repair and overhaul support to U.S. Army PHOENIX, Oct. 5, 2015 – Honeywell Aerospace (NYSE: HON) has been selected to provide additional engine repair and overhaul support for its T-55 turboshaft engine on the U.S. Army’s Chinook helicopters. The repair and overhaul work, which is performed in South Carolina, assures Chinook operators that Honeywell’s turboshaft engines will perform with the power, reliability and payload capability needed for a wide breadth of missions in the Army’s latest cargo helicopters.“The Chinook caters to a wide array of missions for the U.S. Army and needs an engine that supports this. With more than 12 million hours of operation on both the CH-47 and MH-47 fleets, our T-55 turboshaft engine has proved it’s prepared to support Chinook operators wherever the mission takes them,” said Carey Smith, president, Defense and Space, Honeywell Aerospace. “Our commitment extends well beyond the initial delivery of our engines. Our team at the Honeywell Greer facility is equipped with the repair and overhaul expertise to limit the downtime of the Chinook and maintain the extraordinary level of performance that the U.S. Army has come to expect from the T-55.”As tactical challenges grow and the role of the Chinook expands, Honeywell’s T-55 turboshaft engine has helped advance the helicopter’s performance. Equipped with two of Honeywell’s T-55-714 engines, modern variants of the U.S. Army’s Chinook have three times more lift than the original helicopters fielded in the 1960s, are capable of lifting five tons, and have the available power (4,800 shaft horsepower) needed to maintain flight with only one engine. For Chinook pilots, this level of field reliability, power and performance has made the T-55 a valuable tool for the breadth of diverse Army cargo missions, from high and hot operating environments in Afghanistan to the polar regions of Alaska. Supporting Resources- Read more about Honeywell Aerospace and visit our Follow the Aero blog- Like Honeywell Aerospace on Facebook- Follow @Honeywell_Aero on Twitter - Subscribe to Honeywell’s Corporate RSS feedHoneywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel-efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics, and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2015 Honeywell.