Vroom Vroom... Jesse James Unveils His Dodge Polara

Honeywell Garrett pairs up with Roadster Shop and the famous motorcycle builder on his 1500HP Hot Rod

Car and motorcycle builder Jesse James unveiled his latest  -- a one-off, twin-turbocharged 1964 Dodge Polara.

Honeywell Garrett along with custom car builder Roadster Shop made the big reveal at the Specialty Equipment Market Association (SEMA) Show in Las Vegas, NV.

Here are the details: Jesse’s Polara is powered by a 426ci Wegner Motorsports-built Hemi, with a custom intake manifold and titanium turbo manifold, connected to twin Honeywell Garrett GTX3582R turbochargers. Cooling is handled by an air-to-water intercooler and a radiator built by Ron Davis. To put the power to the ground, the Mopar utilizes a Tremec T-56 transmission modified by Blower Transmission, coupled with a Driveshaft Shop driveshaft and a Strange Engineering rear end.

One of the standout upgrades on the completely stripped interior is the set of bespoke fiberglass seats mounted to custom bead-rolled floors, matched perfectly to gauges by Classic Instruments.

SEMA 2017
The 1964 Polara with a simple and clean interior including custom seats, hand-fabricated floorboards, dash, and engine bay, a harness bar, a central switch panel, and custom gauges

On the outside, the 19” wheels provided by Forgeline are wrapped with Nitto NT505R tires, backed by 14” Baer brakes to offer plenty of stopping power for the big sedan. Bringing the entire build together is Roadster Shop’s signature Fast Track chassis with Penske coilovers and splined rear sway bars, giving the car completely modern handling characteristics.

 

Tim Coltey

Marketing Specialist, Garrett® Performance Products - Honeywell Transportation Systems