Positive Energy: This Command Center Turns Hazardous Waste into Clean Power
Here's how BASF is envisioning a green future for chemical waste
April 21, 2018
Chemical products are a key part of everyday life with more than 100,000 substances available and in use around the world. According to data from the UN Environment Program (UNEP), the global chemical industry produces more than 400 million tons of hazardous waste annually. These residues can present a severe threat to health and the environment if not discarded safely and quickly. Chemical company BASF is tackling this challenge in an innovative way: converting chemical waste into reusable energy. The company recently upgraded its central waste incineration plant, which processes all the chemical waste from its site in Ludwigshafen, Germany, the largest chemical production site in the world with more than 250 plants, as well as from outside of the complex. The upgrade completely modernized the 60-year-old incineration control room with our Experion technology.
Here is a behind the scenes look at this state-of-the-art facility to see how it works:
Monitor temperature and pressure
Nearly 30 controllers were installed to handle thousands of input and output signals from the incineration process each day. These signals help plant operators monitor the temperature, flow, level and pressure of the combustion process used on hazardous chemical waste. Once the waste is burned, the generated heat is converted into steam, which is then placed under high pressure in turbines to generate electricity—turning hazardous waste into clean energy.
Visualize from end-to-end
Fully integrated into the consoles are live video feeds from several points of the incineration plant such as the boiler, combustion chamber and turbine. Barco OpSpace provides integration of video and interactive (third-party) computer sources into the Experion Orion console workspace, with control from one keyboard and mouse. A complete visualization of operations at any given moment offering insight into the incineration process from the beginning to the end.
Get real-time information
Operators and production staff use two Collaboration Stations to access a large variety of plant information and documentation in real time — for example electricity and steam reports that provide important updates about how effectively the plant is converting hazardous waste into clean energy.
Keep an eye on it all
The incineration plant is responsible for burning hazardous chemical waste that cannot be recycled or reused in other production processes. These residues are introduced into the plant via pipelines, tanks and containers – mostly from the site itself but also from other nearby facilities. With these systems, plant operators monitor and control devices and equipment, while continuously receiving information on variables such as temperature, pressure and flow.
Copyright © 2021 Honeywell International Inc.
- USA - English
- Algeria - English
- Angola - English
- Australia and New Zealand - English
- Austria - German
- Belgium - Dutch
- Belgium - French
- Brazil - Portuguese
- Bulgaria - Bulgarian
- Canada - English
- Canada - French Canadian
- Czech Republic - English
- Denmark - Danish
- Finland - Finnish
- France - French
- Germany - German
- Egypt - English
- Hungary - Hungarian
- India - English
- Indonesia - Indonesian
- Japan - Japanese
- Kenya - English
- Korea - Korean
- Malaysia - English
- Mexico - Spanish
- Morocco - French
- Nigeria - English
- Norway - Norwegian
- Philippines - English
- Poland - Polish
- Romania - English
- Saudi Arabia - English
- Slovakia - Slovak
- South Africa - English
- Switzerland - French
- Switzerland - German
- Thailand - English
- Tunisia - French
- Turkey - Turkish
- United Arab Emirates - English
- United Kingdom - English
- Vietnam - Vietnamese