Honeywell Helps Cut Energy & Water Consumption at Letterkenny Army Depot for $4.1 Million in Annual Savings


LEAD 3x2To help improve the long-term vitality of an important military installation, Honeywell and the U.S. Army have announced a $43.6-million infrastructure modernization project at Letterkenny Army Depot (LEAD). The project will provide critical improvements and upgrades at the Pennsylvania facility, which is the premier location for maintenance of air defense and tactical missile ground support equipment used by the Department of Defense.  It is expected to cut energy use more than 25 percent, reduce water consumption nearly 50 percent, and generate approximately $4.1 million in annual energy and operational savings.
 
The upgrades are part of a 20-year energy savings performance contract awarded by the U.S. Army Corps of Engineers, Engineering and Support Center in Huntsville, Ala. The contract allows the Army to make extensive improvements at LEAD without an upfront capital investment or additional taxpayer dollars. The work is backed by a financial firm and Honeywell guarantees the upgrades can generate the projected savings necessary to repay the loan, creating a self-funded project. In addition to producing immediate results, the project is a critical step for LEAD in meeting the requirements of a Presidential Executive Order, which calls for federal facilities to reduce energy consumption 30 percent by 2015.
 
“For more than 70 years, this depot has proven its role as a critical support center for our armed forces,” said Col. Victor Hagan, commander for Letterkenny Army Depot. “This work will help us continue our legacy. Improving key infrastructure and technology provides the means to boost efficiency and effectiveness, and maintain the vitality of the organization.”