Product line now includes refrigerants for supermarket, chiller and air conditioning systems with lower global warming potentials than the refrigerants they replace

MORRIS TOWNSHIP, N.J.,Jan. 26, 2015 /PRNewswire/ -- Honeywell (NYSE: HON) today announced the launch of four new lower-global-warming-potential (GWP) products for applications ranging from supermarket refrigeration to industrial cooling.

The new products further expand Honeywell's Solstice line of hydrofluoro-olefin (HFO) refrigerants, blowing agents, aerosol propellants and solvents. Solstice products offer lower global warming potentials with similar or better cooling performance when compared to previous-generation products.

"Each year, the world uses more than 200 million pounds of refrigerant, enough to keep food fresh in 240,000 supermarkets and to cool more than 300,000 commercial buildings," saidGeorge Koutsaftes, global business director for Honeywell's Fluorine Products business. "Honeywell is committed to continuing to invest in the development and introduction of new offerings, to make it easier for industry to adopt and use alternatives to higher global warming potential refrigerants."

Honeywell's new offerings include:

Solstice zd: a nonflammable HFO refrigerant with a GWP equal to 1, for use in low pressure centrifugal chillers, which are most often used to cool large buildings. Trane, a leading air conditioner manufacturer, has already announced that it will use Solstice zd in its new Series E CenTraVac large capacity centrifugal chillers inEurope, theMiddle East and other 50hz markets. Solstice ze: an HFO refrigerant that can be used in equipment that traditionally used R134a (i.e., chillers and refrigeration equipment). Solstice ze offers a GWP of less than 1, which is 99.9 percent lower than the GWP of R134a. Solstice N13: an HFO blend for chillers, as well as medium-temperature applications such as supermarket display cases and self-contained refrigeration units that require a non-flammable refrigerant solution. Solstice N13 is designed to replace R134a and offers a GWP that is 60 percent lower than the GWP of R134a. Solstice N40: an HFO blend for low- and medium-temperature refrigeration equipment such as supermarket freezer cases. Solstice N40 is designed to replace HCFC R22 and HFC R404A, and offers a GWP that is 66 percent lower than R404A. In supermarket trials conducted in the U.S. andEurope, Solstice N40 demonstrated three percent lower energy consumption in low-temperature applications and 5 to 16 percent lower energy consumption in medium-temperature applications as compared to R404A. In addition to its industry-leading Solstice line, Honeywell's Fluorine Products business manufactures and supplies non-ozone-depleting Genetron refrigerants used by top air-conditioning, automotive and refrigeration equipment manufacturers worldwide, blowing agents for energy-efficient rigid foam insulation, and hydrofluoric acid and precursors for nuclear fuel.

For more information on Solstice refrigerants, visit www.honeywell-refrigerants.com.

Summary Table: New Honeywell Solstice Refrigerants

Solstice Product

Designed to Replace:

End-Use Application

Benefits:

Solstice zd

(R1233zd)

R123

Centrifugal chillers

Non-ozone-depleting

GWP of 1; 99% lower than HCFC-123 and 99.9% lower than R134a

Non-flammable (ASHRAE A1)

Solstice ze

(R1234ze(E))

R134a

Chillers and refrigeration equipment

Non-ozone-depleting

GWP of less than 1, 99.9% less than R134a

Solstice N13

(R450A)

R134a

Chillers and medium-temperature refrigeration

Non-ozone-depleting

GWP is 60% lower than R134a

Non-flammable (ASHRAE A1)

Solstice N40

(R448A)

R404A

Low- and medium-temperature refrigeration

Non-ozone-depleting

GWP is 66% lower than R404a

5-16% lower energy consumption in end-use applications

Non-flammable (ASHRAE A1)

Honeywell Performance Materials and Technologies (PMT) is a global leader in developing advanced materials, process technologies and automation solutions. PMT's Advanced Materials businesses manufacture a wide variety of high-performance products, including environmentally friendlier refrigerants and materials used to manufacture end products such as bullet-resistant armor, nylon, computer chips and pharmaceutical packaging. Process technologies developed by PMT's UOP business (www.uop.com) form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel, petrochemicals and renewable fuels. PMT's Process Solutions business (www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas, refining, pulp and paper, industrial power generation, chemicals and petrochemicals, biofuels, life sciences, and metals, minerals and mining industries.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission. Media Contacts: U.S. Jeannine Sohayda 973-455-2706 jeannine.sohayda@honeywell.com Europe Martin Orsag +4 2024 244 2279 martin.orsag@honeywell.com Asia Julia Zhu +86 21 2894 5054 julia.zhu1@honeywell.com