Media Contact


Mike Stoller

Transportation Systems

+1 734 392 5525

+1 734 233 5622 - Mobile

Email


• Seven popular Garrett by Honeywell performance turbos get horsepower range increases
• New compressor wheel aerodynamics key to adding power to trusted Garrett performance


LAS VEGAS, Oct. 31, 2016 -- Honeywell (NYSE: HON) today announced the Nov. 1, 2016, availability of its Garrett GTX Series Gen II Turbochargers featuring updated compressor aerodynamics and additional features resulting in class leading efficiency and horsepower ratings. 

The new upgrades enhance a range of turbo sizes, and starts with fully machined wheels using state-of-the art aerodynamic tools and processes derived from Honeywell Aerospace which develops jet engines and produces some of the most efficient wheels in the industry.

In addition to the newly designed aerodynamics, the next generation of GTX turbos comes with a machined speed sensor port (Garrett speed sensor sold separately) to support tuning and data acquisition and save time and money during installation. It also eliminates additional handling and drilling by a third party which could inadvertently damage the turbo or negatively affect its calibrated performance.

“The new lineup of Garrett GTX Gen II turbos is our most significant portfolio refresh in nearly a decade. We are using advanced technology connected under the larger umbrella of our Honeywell Aerospace business to help design and manufacture turbo solutions that have made Honeywell a turbo leader for more than 60 years,” said, Eric Fraysse Aftermarket vice president and general manager at Honeywell Transportation Systems. “Coupled with the reliability and durability synonymous with the Garrett brand, the increased power range jumps Garrett to the head of the performance enthusiast class.”

Standard features of the Garrett GTX Series Gen II lineup include water-cooled center housing rotating assemblies, ceramic ball bearings for additional responsiveness, new high-flow compressor housings, a fully machined compressor housing inlet, ported shroud, and outlet, and several options for turbine housings to ensure proper installation.

Garrett GTX Series Gen II Maximum Horsepower  HP Increase
GTX2860R 475 hp 75 hp
GTX2867R 550 hp 70 hp
GTX3071R 560 hp 110 hp
GTX3076R 750 hp 110 hp
GTX3576R 750 hp 150 hp
GTX3582R 850 hp 100 hp
GTX5533R 2,500 hp 700 hp

The new GTX Gen II lineup is fully backward compatible and completely interchangeable with first GTX GEN I products and even Garrett’s standard GT product line. In addition to the performance upgrades, the finish of the castings has also been updated to be more uniform reflecting the quality in the product.

Supporting Resources
• Get More Product Info at the Garrett by Honeywell website 
• Follow Garrett by Honeywell on Instagram
• Follow Honeywell Transportation Systems & @Honeywell_Turbo on Twitter

###
About Honeywell Aerospace
Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials.  For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.