Media Contact


Gwennie Cheung

Aerospace

+1 (646) 589-1741 - Mobile

Email

Honeywell Survey: Airlines Risk Losing Passengers Due to Poor Wi-Fi

Consistent, fast connections on flights influence passengers’ airline choice 


Reliable connections on flights anywhere in the world and fast speed to stream audio or video are essential to passengers’ Wi-Fi experience
• More millennials than older generations have switched from their preferred airline to an airline that has better in-flight Wi-Fi options
• Lack of in-flight Wi-Fi has become intolerable as passengers shared they would be disappointed or frustrated without access to this service


PHOENIX, July 12, 2016 – A survey of airline passengers by Honeywell (NYSE: HON) reveals more than increased frustration with current in-flight Wi-Fi offerings compared with the company’s 2014 study. Nearly 3 of 4 passengers are ready to switch airlines today to have access to a faster and more reliable Wi-Fi connection. In addition, out of more than 1,000 American travelers polled, annoyance is growing, with just 22 percent reporting their in-flight Wi-Fi to be extremely reliable over the past 12 months, a dip from 27 percent in 2014.

Travelers have made it clear they expect consistent, faster in-flight connections, and this survey reveals three key reasons why airlines must act quickly to deliver this service or risk losing business.

Traveler Loyalty Lies With Wi-Fi

When traveling, passengers expect a reliable connection to stay in touch with their friends and family, get work done, or be entertained. If that means selecting another airline over their preferred choice, they will do it. More than 1 in 5 (21 percent) have already abandoned their preferred airline for an option with better in-flight Wi-Fi (up from 17 percent in 2014). In-flight service is clearly top of mind for passengers and impacts the way more than two-thirds (68 percent) of travelers book their flights.

Consistent Connections Are Critical Everywhere

With the rise in personal electronic devices, consumers expect reliable connectivity anywhere, including while in flight. Six in 10 (60 percent) travelers surveyed say they would most likely feel disappointed or frustrated if they got on a plane that did not have in-flight Wi-Fi. Even more, 84 percent of travelers, say it is important to have an experience identical to what they have at home or in the office. Most travelers find it essential to experience a reliable connection throughout their entire flight anywhere in the world (90 percent), and one that is fast enough to stream audio or video from sites such as YouTube and Netflix (83 percent).

Millennials Value Wi-Fi More Than Most

U.S. millennials — those born between 1982 and 1998 — represent the most connected generation that took part in this survey, and are the first full generation to grow up in the digital age with news, entertainment, commerce and social networks at their fingertips. If airlines want to earn the business and loyalty of one of the largest consumer segments, they must offer the best global in-flight Wi-Fi service. More millennials than older generations (73 percent versus 63 percent) say Wi-Fi availability impacts the flights they book. Because they value a connected experience more than older generations, more millennials find it important to have fast speed to stream content (89 percent versus 77 percent), and more than 1 in 4 have switched from their preferred airline to an airline with better in-flight Wi-Fi options (27 percent versus 15 percent).

“Passengers are serious about getting the best in-flight Wi-Fi experience possible. To avoid losing passengers and revenue, airlines need a connectivity service that is reliable all the time, no matter where they fly,” said Carl Esposito, vice president, Marketing and Product Management, Honeywell Aerospace. “Travelers do not need to wait any longer for this experience; it is available now. Honeywell has worked with Inmarsat to offer the world’s first global, fast service — GX Aviation — to give passengers reliable in-flight Wi-Fi, anywhere they fly.”

GX Aviation Wi-Fi Keeps Travelers Connected Everywhere

GX Aviation, the first high-speed wireless broadband service to span the world, is the only solution for airlines available right now to provide a constant, high-speed connectivity signal that follows airplanes and passengers flying anywhere in the world. Whether travelers are over land or water, they will have a similar Wi-Fi experience as they would have on the ground. GX Aviation is powered by Honeywell’s JetWave onboard hardware and Inmarsat’s Global Xpress Ka-band satellite network.

Imagine a global cell phone signal from a single provider that follows users wherever they go rather than requiring the users to choose different carriers and different experiences. GX Aviation makes this a reality for in-flight Wi-Fi and is unlike anything else available today. One service provider, one experience, no matter where you are.

About the Survey

The Honeywell Aerospace Connectivity 2016 Survey was conducted by Kelton Global between April 11‒20, 2016, among 1,008 Americans ages 18 and over who have used in-flight Wi-Fi in the last 12 months, using an e-mail invitation and an online survey. Results of any sample are subject to sampling variation. The magnitude of the variation is measurable and is affected by the number of interviews and the level of the percentages expressing the results. In this particular study, the chances are 95 in 100 that a survey result does not vary, plus or minus, by more than 3.1 percentage points from the result that would be obtained if interviews had been conducted with all personas in the universe represented by the sample. The margin of error for any subgroups will be slightly higher.

Supporting Resources
•Read more about Honeywell Aerospace on the Follow The Aero blog
•Like Honeywell Aerospace on Facebook

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel-efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics, and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2016 Honeywell.