Check icon

Success

Your request has been successfully submitted.

Honeywell Expands Stryker™ Controller Portfolio to Bring Increased Application Flexibility

Honeywell Expands Stryker™ Controller Portfolio to Bring Increased Application FlexibilityJan 08, 2014MINNEAPOLIS Honeywell (NYSE: HON) announced today the expansion of its configurable Stryker™ controller portfolio with the addition of the Stryker CVAHU model. Now contractors have the ability to provide control for both variable air volume (VAV) and constant volume air handling unit (CVAHU) applications.Honeywell's Stryker controllers provide off-the-shelf configurability so contractors can engineer a job faster. Stryker is the controller line contractors want when the engineering and installation need to be done quickly. Not every job requires a fully programmable controller like Honeywell's powerful Spyder™ controller, and custom programming for every job can potentially slow the overall install down reducing contractor's bottom line. Stryker is a robust controller that can be easily installed. Its off-the-shelf configurations will be functioning in seconds. Benefits of a Stryker controller include:
  • Reduced engineering time
  • Configurable through a Zio® or Zio® Plus wall module or over the network
  • Two additional accessory loops for flexibility, as needed
  • Ability to create custom sensor tables so existing sensors can be used
  • Available for CVAHU or VAV applications
"Stryker CVAHU continues the evolution of our configurable controller line," said Tom Rosback, General Manager of Commercial Control Systems at Honeywell. "Contractors don't always want or need the full flexibility and custom programming that comes with programmable HVAC controllers. Contractors are busy and they need to get on and off the job quickly and Stryker provides just that."For more information about Honeywell's new additions to the Stryker™ portfolio, please visit www.buildingcontrols.honeywell.com.Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.