Check icon

Success

Your request has been successfully submitted.

Honeywell Fleet Tracking System certified for new helicopter platforms

Sky Connect Tracker III delivers unmatched fleet communications and improves operational safety for global helicopter operators ANAHEIM, Calif., Feb. 25, 2014 – Sky Connect Tracker III is the first system that enables simultaneous worldwide automated tracking, text messaging and voice capabilities to improve crew and passenger safety and increase aircraft availability. The all-in-one voice, text and tracking system from Honeywell Aerospace (NYSE: HON) has received FAA Supplemental Type Certificates for the Sikorsky S-76, AgustaWestland AW139 and Airbus AS350 rotorcraft platforms.“Sky Connect Tracker maintains voice, text and tracking communications for thousands of aircraft operated worldwide and is now expanding its services for three key helicopter platforms,” said Paul West, sales director at Honeywell Aerospace. “Sky Connect Tracker III provides helicopter operators with the crucial information to keep their fleet safe and efficient. Our dual redundant servers currently handle more than 5 million tracking, text and telemetry messages each month, and we expect this number to grow as more customers realize that Sky Connect Tracker III is the best solution for Iridium-based asset tracking and connectivity needs.”Using the Iridium satellite network, Sky Connect Tracker III allows for real-time communication in situations such as:• Alerting ground personnel and crew if an aircraft deviates from a planned flight path• Providing alerts if an aircraft enters a restricted area• Real-time notification of maintenance needs to ensure that the correct maintenance personnel are on hand to perform checks upon landing • Maximizing efficiency of flight operations by tracking the location of the entire fleet at any time• Close monitoring of when, where and how an aircraft is flown for aircraft leasing operationsHoneywell Aerospace is exhibiting at Heli-Expo 2014 in Anaheim, Calif., Feb. 24–27, 2014. To learn more about Sky Connect Tracker III and other systems to enhance the safety and efficiency of your fleet, visit with Honeywell at Booth #6502. Supporting Resources• Read more about Honeywell Aerospace• Read more about Honeywell at Heli-Expo 2014• Visit Honeywell Aerospace Facebook • Follow @Honeywell_Aero on Twitter • Subscribe to Honeywell’s Corporate RSS feedThousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. For more information, visit http://aerospace.honeywell.com or follow us at @honeywell_aero on Twitter.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2014 Honeywell. Media Contact:Nathan DrevnaHoneywell Aerospace(202) 662-2672 nathan.drevna@honeywell.com