Check icon

Success

Your request has been successfully submitted.

RAE Systems Introduces First Wireless, 4-Gas Pumped and Diffusion Monitor For Real-time Industrial, Oil & Gas and Emergency Response Gas Detection

QRAE 3's advanced wireless functionality delivers hazard data 24/7/365 to increase worker, asset, and responder safety San Jose, Calif. – February 10, 2014 – RAE Systems Inc., the leader in wirelessly connected gas and radiation detection solutions, today introduced the industry’s first wireless, portable, 4-gas pumped and diffusion gas monitor that will significantly enhance worker safety in industrial environments and better protect first responders.RAE Systems’ new QRAE 3 is a versatile, rugged, one- to four-sensor gas monitor that provides continuous exposure monitoring of oxygen (O 2), combustibles, and toxic gases, including hydrogen sulfide (H 2S), carbon monoxide (CO), sulfur dioxide (SO 2) and hydrogen cyanide (HCN). The QRAE 3 is certified for use in hazardous environments, and is designed for use across a broad array of industries where exposure to toxic gas is a constant safety threat. These industries include a broad range of industrial, oil and gas, environmental, first responder and national defense applications.When a situation arises, safety officers must make critical, split- second decisions about how and where to deploy resources. They need access to real-time threat data, which QRAE 3 can provide, to help make faster, more informed decisions to protect lives and property.The QRAE 3’s wireless communication capability enables access to real-time, remote instrument readings and alarm status – including an innovative “Man-Down” alarm – from any location, for better visibility and faster response. Real-time hazard readings can also be communicated to the ProRAE Guardian Safety System and the EchoView Host Closed-Loop Wireless System for safety-enhancing wireless monitoring outside the hot zone, from a plant safety office or from a remote, enterprise location. This can help facilitate faster, data-driven decision making to alert responders, save lives and protect assets.“RAE Systems has been the industry leader in advancing wireless gas detection technologies that help save lives and assets for more than a decade,” said Thomas Negre, vice president of Products and Marketing for RAE Systems. “With the addition of the QRAE 3, RAE Systems now offers the most extensive line of area, survey and portable wireless gas detectors making affordable, cutting edge toxic gas detection solutions available to more customers across a broader range of applications. Our wireless monitors include single-gas, 4-gas, multi-gas with gamma (radiation detector), transportable multi-gas with gamma and semi-fixed with gamma for enhanced organizational safety.”“The toxic vapors present in fire smoke, particularly hydrogen cyanide and carbon monoxide, the “Toxic Twins,” are increasingly recognized as the most dangerous and deadly part of any fireground operation. As such, it is essential for incident commanders to have access to critical, real-time threat data to help protect personnel from dangerous exposure levels,” said Jason Krusen, Chief of Special Operations at Columbia, SC, Fire Department and President of the FireSmoke Coalition. “With the QRAE 3, emergency responders now have wireless access to Toxic Twin gas information, which can help protect their long-term health and safety.” QRAE 3 Breakthrough TechnologyThe QRAE 3 offers breakthrough gas detection features and capabilities, including:
  • Advanced wireless functionality – First and only solution that is rapidly deployable in both closed-loop and global, 24/7 Internet-based systems.
  • Enhanced organizational safety and compliance – Organizations can leverage policy enforcement features (RAE Systems AutoRAE 2 bump and calibration stations) to ensure users follow calibration and bump test procedures and that their instruments are working properly. The QRAE 3’s AutoRAE 2 Cradle will be available during the first calendar quarter of 2014.
  • Protection Against the “Toxic Twins” The QRAE 3 is the only gas monitor that provides a wireless fire smoke configuration to detect for the “Toxic Twins” (CO and HCN).
  • Advanced User Interface – The QRAE 3 features large graphical display, icon-driven user interface through intuitive, two-button operation. The QRAE 3 also includes a “Man Down” alarm and automatic flip screen. All ToxiRAE Pro, MultiRAE and QRAE 3 monitors now feature a similar menu, navigation and icons.
  • Available in Multiple, User-configurable Monitors – All configurations are available pumped or diffusion, and wireless or non-wireless, and with various sensor configurations. The QRAE 3 includes a three-year warranty on standard sensors.
  • Compatible with RAE Systems wireless safety systems – QRAE 3 real-time threat data can be monitored on mobile devices via the ProRAE Guardian Wireless Safety System, 24/7, through a secure Internet connection, or via the EchoView Host Closed-Loop Wireless System.
AvailabilityThe RAE Systems QRAE 3 will be available in North America in February 2014. The QRAE 3 will be available with ATEX, CSA, IECEx certification worldwide beginning in March 2014. Learn More, See More
  • For more information on the QRAE 3 and to schedule a demonstration, click HERE.
  • To watch a video on Wireless Plant-Wide Safety that includes the QRAE 3, click HERE.
  • For more information and to see how to monitor toxic industrial chemicals, flammable gases, VOCs, radiological, man-down, meteorological and physiological information from outside the hot zone via the ProRAE Guardian Wireless Safety System, click HERE.
  • To watch a video on the hazards of the Toxic Twins (HCN and CO) in fire smoke, click HERE.
### About RAE Systems Inc.RAE Systems innovates, designs and manufacturers gas sensors and radiation detectors. The company offers a full line of fixed and portable gas detection solutions, including handheld and personal chemical, compound and radiation detection instruments. RAE Systems’ real-time safety and detection systems have been deployed by organizations in the oil and gas, fire and HazMat, industrial safety, national security and environmental markets, helping save lives and maintain safety in 120 countries. The company’s industry-leading gas sensors and radiation detection solutions are widely recognized for their performance and reliability. Learn more at raesystems.com.On June 4, 2013, Honeywell (NYSE: HON) completed its acquisition of RAE Systems Inc. The company will be integrated into Honeywell Analytics, part of Honeywell Life Safety (HLS) within Honeywell Automation and Control Solutions (ACS). Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.