Check icon

Success

Your request has been successfully submitted.

Honeywell's TruStability Pressure Sensors Chosen by SMAY for their iSWAY-FC Series Compact Pressurization Units

The Polish Company, a Leading Supplier of HVAC Systems, Chose Honeywell's Pressure Sensors Due to Their Stability, Accuracy and Fast Response Time, Helping to Ensure Building Safety. MINNEAPOLIS, March 17, 2014 Honeywell (NYSE:HON) today announced that SMAY, a leading Polish manufacturer and supplier of HVAC systems, has chosen the company's TruStability® board mount pressure sensors with diagnostic function and digital output to monitor differential pressure for variable air volume control, static duct pressure, clogged filter detection, transmitters, and indoor air quality.Honeywell Sensing and Control (S&C) provided the sensors that are used for the iSWAY-FC series compact pressurization units, designated for overpressure protection of both vertical and horizontal escape routes in the various buildings in case of fire. Due to the applied control system and wide range of accessories, these units can be used to protect spaces even with a complicated building design, with different cubature like lift-shafts or stairs. Due to its compact design and structure, the iSWAY-FC series compact pressurization units can be assembled almost anywhere inside the building, like technical floors, roof level or ground level."We chose Honeywell because SMAY guarantees the highest level of quality and safety of its products" said Marzena Maj, commercial director of SMAY. "This is why we collaborate only with suppliers that provide the most innovative, technically advanced, high-quality products."According to the energy efficiency European directive 2012/27/EU, by 2020 the European Community targets to reach 20% energy savings, especially in buildings, by improving the thermal isolation. In order to meet this goal, a new generation of sealed buildings using air control systems must allow drastic reduction of energy consumption. To keep these buildings safe in case of fire, an overpressure system is needed to protect the critical places within a building.In order to ensure building safety and overpressure protection against fire for customers with different needs, SMAY needed very accurate, fast and stable pressure sensors to monitor differential pressure and detect overpressure in case of fire.Honeywell's pressure sensors were chosen after a rigid selection process and extensive testing where they provided the most stable output and an insurmountable reaction time of less than 2 seconds. The customer benefits from a very stable system, even under difficult conditions like a complicated building design or during a fire. Due to Honeywell's TruStability® board mount pressure sensors, the iSWAY-FC series compact pressurization units produce the set value of overpressure within the space of a staircase, shaft or rescue elevator or in a system of separate elevator shafts, each with its own air supply source. The sensor can also control the pressure in the air supply duct."We are very proud that our sensors offer SMAY a competitive advantage and help its customers safely operate their buildings, even during a fire," said Remi Volpe, vice president and general manager of Honeywell Sensing and Control in EMEA. "This is a confirmation that our high-quality pressure sensors provided stability under both normal and, more importantly, critical working conditions such as a fire, which is crucial for life and safety."Honeywell's TruStability® board mount pressure sensors combine high sensitivity with high overpressure and burst pressure that provides flexibility in sensor implementation and reduces design requirements for protecting the sensor. Honeywell's TruStability® board mount pressure sensors offer customers industry-leading, long-term stability, minimizing system calibration needs and maximizing system performance), industry-leading total error band (providing the sensor's true accuracy and eliminating individual testing and calibration of every sensor) and industry-leading accuracy, thus reducing software needs to correct system inaccuracies and minimizing the system design time. View all Honeywell Sensing and Control press releases Learn more about Honeywell Sensing and Control About SMAY SMAY LLC is a as Polish consulting and production company that since 1989 has provided ventilation solutions and devices to improve comfort and safety in buildings. The company provides solutions for fire ventilation systems, overpressure protection systems against smoking in the means of escape in case of fire, air control systems, air flow control systems in laboratories, air distribution systems and garage fire ventilation. SMAY products are chosen and installed in many prestigious buildings including hotels and trade centers, hospitals, office buildings and industrial facilities. The growing position of the company is also proved by the number of the awards it has received, as well as by the products it offers. About Honeywell InternationalHoneywell ( www.honeywell.com ) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.comFor more information on Honeywell Sensing and Control, visit sensing.honeywell.com .This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.# # # Contact:SMAY LLCGregory Sypek+48 795 575 286g.sypek@smay.euPaula Calarasu Honeywell Sensing and Control+40 724 220342paula.calarasu@honeywell.com