Check icon

Success

Your request has been successfully submitted.

Honeywell Spectra® Fiber Strengthens 745-Foot Vancouver Sculpture By World-Renowned Artist

Biggest sculpture by Janet Echelman to premiere on March 15 in Vancouver, British Columbia MORRIS TOWNSHIP, N.J ., March 13, 2014 Honeywell (NYSE: HON) announced today that its Spectra ® fiber is strengthening the ropes used in a new sculpture making its world premiere this month in Vancouver, British Columbia, by world-renowned artist Janet Echelman.
The fiber, which is pound-for-pound 15 times stronger than steel but light enough to float, gives Echelman's sculpture the strength it needs to sustain winds of up to 96 miles per hour while remaining light enough to attach to existing buildings and eventually be transported around the world to be displayed. The sculpture weighs 3,500 pounds and its first installation will suspend 745 feet across the waterfront between the Fairmont Waterfront Hotel and the Vancouver Convention Center. Echelman is known for creating massive sculptures that respond to the forces of nature. The new sculpture will be of a size and scale never before attempted by Echelman."When I began planning for a sculpture of this size, I knew Spectra fiber would be a critical component in helping me achieve my artistic vision," said Echelman. "The fiber gives my work the strength it needs, but allows me to create a structure that is light and delicate so that it moves with the wind." The ropes are produced by custom rope manufacturer Yale Cordage, which is known for its application-specific ropes and efficient use of fiber to provide maximum strength in its products. Yale created a 12-strand hollow braided rope using Spectra fiber for this project."Spectra fiber's lightweight strength makes it a sought-after material for specialty applications like Janet's innovative and impressive sculpture, but also for critical applications ranging from body armor to slings for lifting bridge components weighing millions of pounds," said Mark Saholsky, global business manager for Honeywell's Advanced Fibers and Composites business. "This Vancouver installation of the artwork underscores the capabilities of Spectra fiber."The sculpture will premiere on Saturday, March 15, 2014, in conjunction with the TED conference's 30 th anniversary.TED is a nonprofit organization devoted to "ideas worth spreading." The organization's conferences bring together the world's most fascinating thinkers and doers, and content spans from topics related to science, business, the arts, and technology, to the global issues facing our world. Echelman was asked to create a monumental aerial sculpture to celebrate TED's 30 th anniversary, an event that will bring together 100 of the best TED speakers of all time, including Echelman. Following the conference in Vancouver, the artist plans to install the sculpture in other locations around the globe.Spectra fiber has been used in several of Echelman's previous works, including her sculpture 1.26, which draws inspiration from the February 2010 earthquake in Chile that shortened the length of the earth's day by 1.26 microseconds by slightly redistributing the earth's mass. To date, 1.26 has been installed on three continents North America, Australia, and Europe and will be installed in Asia later this year. Echelman is a recipient of the Guggenheim Fellowship and was named an Architectural Digest 2012 Innovator for "changing the very essence of urban spaces."Spectra fiber is made from ultra-high-molecular-weight polyethylene using a patented gel-spinning process. The fiber exhibits high resistance to chemicals, water, and ultraviolet light.Industrial applications for Spectra fiber include security netting, rope, cordage, and fishing line, as well as curtains designed to protect windows and doors during hurricanes. The fiber is also commonly used in bullet-resistant armor.Honeywell maintains an active Spectra fiber and ballistic materials research program focused on continuous improvement and development of high-performance materials.For more information about Honeywell Spectra fiber, visit www.honeywell-spectra.com.Honeywell Performance Materials and Technologies is a global leader in developing and manufacturing advanced materials and process technologies. These materials and technologies are used by people every day in a wide range of industries and applications, from petroleum refining to environmentally friendlier refrigerants to bullet-resistant vests. Our advanced materials are critical in the manufacture of products ranging from nylon to computer chips to pharmaceutical packaging. Process technologies developed by our UOP business form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel and petrochemicals. UOP is now pioneering technology to produce real fuels from renewable energy sources.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.