Check icon

Success

Your request has been successfully submitted.

New Honeywell Ultrasonic Flowmeter Helps Achieve 'Metering Intelligence' for Pipeline Monitoring

HOUSTON, March 31, 2014 Honeywell ( NYSE: HON) today released its newest ultrasonic flowmeter designed to help natural gas producers improve efficiency by more-accurately tracking the movement of gas through pipelines. The USM GT400 Ultrasonic Flowmeter helps to reduce the amount of effort needed to maintain pipeline metering, which is especially critical today given the skills shortage many oil and gas companies are facing as veteran engineers retire.Honeywell flowmeters are currently used in thousands of installations worldwide to measure the volume of gas across the supply and value chain. The USM GT400 measures the volume of natural gas at every stage of its movement, storage and utilization, which is important because the volume of gas transported via pipelines to consumers is metered for billing purposes. "As the natural gas industry continues expanding, companies have a tighter margin of error when it comes to lowering operating and capital costs, improving uptime and reducing risks," said Tony Tielen, vice president of Honeywell Process Solutions' Engineered Field Solutions division. "Accuracy is the key to staying within those margins, and the USM GT400 uses a unique blend of multi-path measuring technology, field-proven electronics, sophisticated diagnostics and a user-friendly interface to achieve true metering intelligence."Compliant with CEESmaRT™ technology a secure, cloud-based solution for condition-based monitoring the USM GT400 provides stability during flow perturbations thanks to its direct-path technology with six measuring paths on three levels. The paths are arrayed in an "X" pattern in horizontal planes. This orientation enables measurement of swirl, cross-flow and asymmetry, as well as transparent path velocity weighting per the Gauss-Chebyshev profile model for compressible fluids. The USM's electronics are used to handle path-specific measurements while optimizing internal diagnostics. It includes speed of sound (SoS) and flow velocity calculations, signal processing and data storage capabilities, and can interface to flow computers, gas chromatographs and SCADA systems. The meter's transducer which operates at standard frequencies of 120 or 200 kHz, and alternate frequencies are available for noisy environments consists of piezoelectric crystals fully encapsulated in titanium housing for resistance to dirt. This unique configuration is field-replaceable under pressure. Regulator noise has marginal impact on the flowmeter's measurements, thanks to Honeywell's proprietary, MID-approved detection algorithm, coupled with the unique transducer design. This combination extends signal amplitude for a high signal-to-noise ratio (SNR) versus traditional intrinsically safe transducers. Additionally, Honeywell's patented "live" Precision Adjustment maintains the measurement accuracy of the meter at all times. Windows™-based RMGViewUSM software allows manufacturers to monitor the health of the flowmeter, alerts users to upset conditions, and provides diagnostics for alarming. It also allows direct access to the electronic measuring system via a PC to read out and change parameters, represent measured values, and create test certificates and data sheets.For further information, please visit www.honeywellprocess.com.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Process Solutions is part of Honeywell's Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Process Solutions, access www.honeywellprocess.com. This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.# # #