Check icon

Success

Your request has been successfully submitted.

New Module Makes It Easy to Convert Existing Hardwired Security Systems to Wireless

5800C2W Hardwired to 5800 Wireless Converter Paves the Way to Expand Connected Home and Business Offering with Easy Upgrades to LYNX Touch MELVILLE, NY., March 19, 2014 Honeywell (NYSE: HON) today announced the release of the 5800C2W Hardwired to 5800 Wireless Converter, a device that enables retrofitting existing security control panels of virtually any type or brand by converting wired sensors to Honeywell’s 5800 Series wireless technology. Up to nine hardwired zones can be easily converted to 5800 wireless protection zones eliminating the cost of adding transmitters. The 5800C2W is a reliable solution that lets security professionals expand their connected home and building portfolio by offering Honeywell’s LYNX series of all-in-one security systems to more users. The award-winning LYNX Touch 5100 includes a bright, full-color touchscreen display with intuitive prompts and icons that greatly simplify operation, programming and training. It features 4G/Wi-Fi alarm communications, Z-Wave home automation, garage door control and more. All LYNX systems are compatible with Honeywell Total Connect Remote Services, which provide security professionals with an excellent opportunity to earn additional recurring monthly revenue (RMR). Converting wired zones to wireless reduces installation costs, time and materials. One-button calibration automatically detects EOL resistor value. By using the existing wired infrastructure, installers can eliminate the labor and expense of adding new transmitters to the system’s protection points. A power supply is included letting installers power wired PIRs right out of the box. The 5800C2W is also ideally suited for use in new construction installations that have been fitted with hardwired systems. Honeywell’s 5800C2W is available through security dealers across North America. For more information, please call 1-800-467-5875 or visit www.honeywell.com/security. Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
Ralph Maniscalco Honeywell 516-577-2803 ralph.maniscalco@honeywell.com
Andres Ybarra Weber Shandwick 952-346-6314 aybarra@webershandwick.com