Check icon

Success

Your request has been successfully submitted.

Comfort When You're Home, Savings When You're Away: Introducing Honeywell's Lyric™ Thermostat

The Thermostat That Recognizes Your Family's Busy Lifestyle, Heating And Cooling Your Home Based On Smartphone Location MINNEAPOLIS, June 10, 2014 There's no such thing as a regular routine for today's busy families. No two days are alike and schedules change by the minute. Honeywell (NYSE: HON), the leader in managing home comfort and security for 125 years, is today launching the LyricTM thermostat to put you back in control. The Lyric thermostat knows when you are coming and going, based on smartphone location, to deliver comfort when you're home and savings when you're away.The Lyric thermostat is the first offering in a new family of innovative connected home products from Honeywell, the recognized category leader found in more than 150 million homes globally. The Lyric thermostat is designed for how people really live today:
  • Using the location of your smartphone, the geofencing feature automatically turns the Lyric thermostat into energy saving mode when a home is empty, and then senses when you are coming home and heats or cools the house to your preferred temperature.
  • The Fine Tune feature factors indoor and outdoor temperature, humidity, and weather into its algorithm, enabling it to provide the most comfortable temperature for homeowners. No other do-it-yourself Wi-Fi thermostat on the market today does that.
"Most people don't have a predictable pattern to how they live their lives; why not have a thermostat that adjusts based on your real-time schedule?" says Beth Wozniak, president of Honeywell Environmental and Combustion Controls. "With the Lyric thermostat's geofencing capability, my house returns to my preferred comfort setting when I'm within a few miles fromhome. Quite simply, the Lyric thermostat offers me the ability to keep my life in tune delivering comfort when I'm home and savings when I'm gone."Beyond a smartphone, the temperature can be managed using Honeywell's familiar round dial control on the thermostat itself. With the Lyric app (available via the App Store on iTunesTM and Google PlayTM), homeowners can adjust their home's temperature to life as it happens, wherever they are. When a homeowner walks up to the Lyric thermostat, a built-in proximity sensor signals the display to turn on and show current temperature and the home's heating or cooling status. A soft halo of light in orange (heating), blue (cooling), or green (away/energy savings) momentarily illuminates around the thermostat to indicate it is making temperature adjustments. Additionally, touch-sensitive buttons flank the center display one for accessing current and upcoming weather information, and one for setting back your temperature while you're away. The Lyric thermostat provides easy-to-understand alerts on when to change a filter, if and when your furnace needs servicing, and even help find a trusted service professional.The gloss white finish and silver accents of the Lyric thermostat, along with its shallow depth and flush wall mount, add a contemporary appearance to any room. Beyond contemporary design and innovative functionality, it delivers the same reliable control and accuracy for which Honeywell is known since it introduced the iconic Round®' in 1953.The Lyric thermostat is available now via professional heating and cooling contractors, and will be available at retail beginning in August 2014 for $279 (MSRP). To learn more, please visit http://lyric.honeywell.com. Consumers who want installation assistance can search for a local contractor at http://lyric.honeywell.com.