Check icon

Success

Your request has been successfully submitted.

Honeywell's New LYNX Touch 5200 Introduces Live Video On-Demand, Two-Way Voice Over WiFi® and More

All-in-One Home and Business Control System Enhances User Experience, Improves Business EfficiencyMELVILLE, N.Y., June 9, 2014 Honeywell (NYSE: HON) today introduced a new all-in-one system that allows dealers to offer an enhanced user experience while reducing costs the LYNX Touch 5200. Consumers can now view live, IP video on-demand directly on the panel’s 4.7-inch vivid color touchscreen. In addition to two-way voice over GSM, LYNX Touch 5200 offers two-way voice over Wi-Fi® an industry first that dramatically streamlines the installation process, saves money and time and provides greater options for connectivity.Incorporating video right on the touchscreen helps dealers elevate their connected home offering and provide an unrivaled user experience right out of the box, said Robert Puric, marketing director, Honeywell Security Products Americas. By delivering integrated, economical, on-demand video along with innovations like two-way voice over Wi-Fi LYNX Touch 5200 truly takes the all-in-one system to the next level.The unit supports single-camera viewing when used with Honeywell Total Connect Video products: the iPCAM-PT, iPCAM-WO, iPCAM-WI2/B and ACU. With the exclusive Honeywell LYNX Connect app, users can also view live video feeds and control their systems from an iOS or Android device anywhere on premises, even without a Honeywell Total Connect account.A new sunrise/sunset feature can be easily programmed to trigger scenes such as lights turning on and off on a seasonal basis. For an added level of security, Z-Wave® lights can be randomized for an occupied appearance when a home or small business is empty. Additionally, the Night Stay Arming Mode arms preselected interior sensors such as in a basement or on the main floor while letting end users move about freely in areas like hallways or upper floors. Support for Z-Wave® flood sensors has also been added, potentially reducing costly structural damages by shutting down a building’s main water line when water is detected.Remote-upgradeable software eliminates the need for installers to schedule on-site visits, and more intuitive default settings reduce set-up and customization time. LYNX Touch 5200 boasts features ideal for small commercial applications, such as allowing users to set up to 32 individual security codes including an installer code and master code typically assigned to a business owner or the system’s primary administrator or controller.To help market the product, free iOS demo apps let dealers show prospective customers exactly how LYNX Touch 5200 works right on their iPhone® or iPad® without the need for a physical keypad or demo case.For more information, please visit our Dealer Toolkit.About HoneywellHoneywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.Contact:Ralph ManiscalcoHoneywell516-577-2803ralph.maniscalco@honeywell.com