HOUSTON, June 3, 2014 Honeywell (
NYSE:HON) Process Solutions today launched its new range of
SmartLine™ industrial temperature transmitters, which improve overall plant and employee efficiency even in harsh and noisy process environments.This new product line is part of Honeywell's SmartLine field instrument product family, the industry's first modular and most reliable transmitter family currently available for pressure measurement.

"The SmartLine temperature transmitter is based on the same proven platform as our current SmartLine pressure transmitter. They provide our customers with better performance, unique features that lower their total cost of ownership, and the best integration capabilities available when used with our Experion® Process Knowledge System (PKS)," said Don Maness, vice president and general manager, Field Products, Honeywell Process Solutions. "SmartLine helps reduce project costs and startup time, avoid unplanned downtime, improve product quality, and shorten time to repair."
In industrial plants, field instruments that measure temperature are used throughout the manufacturing process to enable operational safety and product quality. Large industrial complexes, such as those for refining crude oil or producing chemical products, can employ thousands of these devices within their manufacturing processes.SmartLine temperature transmitters lower plant lifecycle costs by making it easier to maintain field devices with their unique efficiency-enhancing features such as an advanced graphic display capable of showing process data in graphical formats and communicating messages from the control room. In addition, all SmartLine transmitters, whether they measure pressure or temperature, utilize modular components which simplify field repairs and reduce the parts inventory required to make those repairs. These parts can be easily upgraded and even exchanged between the two different product lines.SmartLine includes several features to ensure plant reliability and safety. For example, the SmartLine temperature transmitter incorporates a dual-compartment housing for maximum robustness. In addition, it features intuitive diagnostics for both the transmitter and sensor. This diagnostic information is also uniquely available on the transmitter display providing a real-time view of the sensor health to support proactive maintenance.To reduce lifecycle costs, the transmitter features a built-in dual-input and digital output option to minimize the number of instruments needed for both monitoring and switching needs. Along with its unique modularity, SmartLine reduces complexity along the entire lifecycle, from avoiding initial purchasing costs to reducing maintenance and inventory expenses by eliminating spare parts requirements and simplifying module replacements and upgrades. "Companies today are trying to do more with fewer experts," Maness said. "The SmartLine platform makes employees more efficient with the ability to use the display to communicate with field personnel. In addition, with the modular design, employees can use similar parts between both pressure and temperature models, making it faster and easier to change a part or upgrade the devices." Employee efficiency features include wiring polarity insensitivity and local configuration capabilities. Unlike most other transmitters, SmartLine transmitters cannot be damaged by reversed loop wiring polarity and will function correctly if reverse connected. This protection significantly helps during a plant startup, when time can be wasted locating and repairing incorrectly wired devices. In addition, an advanced display and local configuration provides capabilities for field operators to configure the device in the field, solve problems and avoid errors with no need for a handheld device.Honeywell's unique Smart Connection Suite control system integration delivers transmitter messaging, maintenance mode indication and tamper alerts to improve field time to repair and control room communication, avoid unit trips and make employees more efficient.For further details about Honeywell's industrial field devices, please visit www.honeywellprocess.com/SmartLine?.Honeywell Process Solutions (www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas; refining; pulp and paper; industrial power generation; chemicals and petrochemicals; biofuels; life sciences; and metals, minerals and mining industries. Process Solutions is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes UOP, a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries.Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.###