Check icon

Success

Your request has been successfully submitted.

NEW HYBRID ENERGY-ABSORBING LANYARD FROM HONEYWELLSIMPLIFIES PROCESS OF CHOOSING "THE RIGHT" LANYARD IN CANADA

SMITHFIELD, RHODE ISLAND, Sept. 16, 2014 Honeywell (NYSE:HON) todayannounced the Hybrid Energy-Absorbing Lanyard the first-of-its-kind fall protection lanyard to meet Canadian Standards Association (CSA) standards for both Class E4 and Class E6. The new Hybrid Lanyard eliminates the guesswork involved in choosing the appropriate lanyard for workers of different weights thereby reducing error and increasing safety for those working at height.The CSA classifies lanyards into two types based on their ability to absorb the kinetic energy from a fall. Class E4 lanyards are designed for lighter workers (100 - 254 lbs.) and Class E6 lanyards are for heavier workers (200 - 386 lbs.). Historically, to meet these requirements, safety managers have either stocked both classes of lanyards, or relied on just one class for use by workers of all weights a practice that is not CSA compliant and is potentially unsafe.As the industry's first lanyard to be CSA certified for Class E4 and E6 (appropriate for workers weighing between 100 - 386 lbs), the new Honeywell Hybrid Energy Absorbing Lanyard is the simple, safe, and fully-compliant solution. The Hybrid Lanyard increases worker safety by eliminating the need to stock and choose between two types of lanyards.The new Hybrid Energy-Absorbing Lanyard is available now, in a variety of styles, from both Miller and North fall protection brands.View the new Hybrid Energy-Absorbing Lanyard video at http://hwll.co/hyrh. For more information, visit http://hwll.co/HybridLanyard, contact your nearest Honeywell Safety Products distributor, or call Honeywell Customer Care in Canada at 1-888-212-7233.[Note to Editors: High-resolution photos for publication of the new Hybrid EnergyAbsorbing Lanyard can be downloaded from http://hwll.co/7d4b.About Honeywell Safety ProductsHoneywell Safety Products (HSP), a global manufacturer of leading personal protective equipment(PPE) and provider of safety solutions, helps company employees make safer decisions on theirown and build an enduring culture of safety. With world class brands such as Honeywell®, Uvex®,North®, Howard Leight®, Miller®, Fibre-Metal® and Servus®, HSP offers a full range of qualityPPE, including: protective clothing; fall and hearing protection products; solutions that protecthands, head, feet, eyes and face; along with respiratory, welding, first-aid, lockout/tagout and trafficsafety equipment. Lead them to safetyvisit www.honeywellsafety.com/culture to learn more.About HoneywellHoneywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturingleader, serving customers worldwide with aerospace products and services; control technologies forbuildings, homes, and industry; turbochargers; and performance materials. For more news andinformation on Honeywell, please visit www.honeywellnow.com.###