Check icon

Success

Your request has been successfully submitted.

Honeywell's Latest Smartline Transmitter Increases Capabilities of 'Smart' Field Products

THE HAGUE, The Netherlands, Nov. 11, 2014 Honeywell (NYSE:HON) Process Solutions (HPS) today announced the launch of the SmartLine® Guided Wave Radar Level transmitter, the latest addition to HPS's SmartLine industrial transmitter family. The new device can measure the level and volume of liquids inside processing tanks up to 160 feet in height.

The high performance SmartLine Guided Wave Radar Level transmitter features industry leading specifications as well as an advanced level of user experience with the introduction of the Application Validation Tool. This online tool allows customers to input technical data about their specific process tank and to validate that the correct level transmitter application is delivered to the site ready to install out of the box.

"The new SmartLine level transmitter leverages the same proven platform, innovative modular design and ease of use as the pressure and temperature transmitters," said Don Maness, vice president and general manager, Field Products, Honeywell Process Solutions. "This helps facilities manage cost by reducing inventory, speeding start-up and, with Honeywell's Application Validation Tool, operators can have complete confidence that the level transmitter ordered will be the correct one for the tank application."

The new level transmitter features a choice of a basic alphanumeric display or an advanced graphics display. The advanced graphics display, capable of showing process data in graphical formats and communicating messages from the control room, also offers multiple languages and full integration with Honeywell's flagship Experion® process control system.

Field instruments are used throughout industrial plants to measure and transmit critical data points from throughout the processes to the control room. Large industrial complexes, such as those for refining crude oil or producing chemical products, can employ thousands of these devices within their manufacturing processes.

The SmartLine instrument line also includes:

SmartLine Temperature transmitters measure temperature accurately and reliably in industrial processes in tough and noisy environments, converting low level signals from temperature sensors to analog and digital output signal

  • SmartLine Pressure transmitters measure absolute pressure, gauge pressure, differential pressure, and flanged and remote seal transmitters. Refineries, chemical and pharmaceutical plants and paper mills around the globe rely on theses transmitters for accurate and consistent pressure measurement.

Honeywell introduced the smarter field device concept with its SmartLine Pressure transmitter, the industry's first modular and most reliable transmitter delivering value across the entire plant lifecycle. Setting a standard for ease of use and total performance in harsh and noisy process environments, the SmartLine family also offers lower total cost of ownership, from reducing initial purchasing costs, providing flexibility for post start-up modifications, reducing maintenance and inventory costs along with high accuracy and stability.

SmartLine transmitters integrate with all control systems, however when integrated with Honeywell's Experion® PKS, operators benefit from these unique advantages:

Extended diagnostics assess the health of critical field assets

  • Maintenance status display confirm the transmitter is in the right mode before maintenance can be performed
  • Transmitter messaging allows the operator to send messages to the transmitters advanced display
  • Tamper alert provides ability to detect unauthorized access of transmitters in remote locations such as pipelines and wellheads.

For further details about Honeywell's industrial field devices visit www.honeywellprocess.com/smartline.

# # #

Honeywell Process Solutions (www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas; refining; pulp and paper; industrial power generation; chemicals and petrochemicals; biofuels; life sciences; and metals, minerals and mining industries. Process Solutions is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes UOP, a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

# # #