Check icon

Success

Your request has been successfully submitted.

Honeywell's Low-Global-Warming Material Insulates Homes In Canada

January 08, 2015

Honeywell's Low-Global-Warming Material Insulates Homes In Canada

Ontario-based Elastochem is the first to use Honeywell's Solstice® Liquid Blowing Agent in spray foam wall insulation in Canada

MORRIS TOWNSHIP, N.J., Jan. 8, 2015 &emdash; Honeywell ( NYSE: HON) announced today that its low-global-warming insulating materials are now being used to insulate homes in Canada.

Elastochem Specialty Chemicals is using Honeywell's Solstice® Liquid Blowing Agent (LBA) in its Insulthane® Extreme spray foam insulation system for residential walls. Solstice LBA, which allows closed-cell spray foam insulation to expand and provides the majority of the foam's excellent insulating properties, provides superior insulating performance with significantly lower global warming impact compared to older technologies.

"Elastochem is focused on making better foam products for customers and the environment," said John Volk, general manager of Ontario-based Elastochem. "Solstice LBA is helping us do just that while cost-effectively meeting current and future energy efficiency and environmental regulations."

Laura Reinhard, global business manager for Honeywell's spray foam business, said closed-cell spray foam is increasingly being used in cold-weather markets such as Canada, where residential construction is growing.

"Closed-cell spray foam insulation seals gaps, cracks and holes as it is applied, making it one of the most energy-efficient insulation products available today," said Reinhard. "Solstice LBA enables advanced wall insulation like Elastochem's Insulthane Extreme system to have a lower global warming potential and better insulating performance."

According to Statistics Canada, residential construction investment totaled $30.2 billion in the third quarter 2014, up 5.9 percent from the same quarter in 2013. Renovation spending was behind most of the increase at the national level, rising 8.9 percent to $13.9 billion.

Solstice LBA has an ultra-low global warming potential of 1, which is 99.9 percent lower than the global warming potential of the most commonly used blowing agent for spray foam, HFC-245fa. According to Elastochem, Solstice LBA provides 7 percent better insulating performance than HFC-245fa. It is used in a range of foam applications, including insulating commercial refrigeration equipment, metal architectural panels, spray foam roofing and energy-efficient refrigerators.

Whirlpool announced in January 2014 that all its U.S.-based refrigerator manufacturing would use Solstice LBA for insulation by the end of the year. Chinese refrigerator manufacturers Midea and Haier have both adopted Solstice LBA to reduce the climate impact and improve the energy efficiency of their refrigerators and freezers. Kingspan Insulation, a leading European manufacturer of rigid insulation products, has also adopted Solstice LBA for use in certain high- and premium-performance insulation panels.

It is a near drop-in replacement for other liquid foam blowing agents and is nonflammable, making it a cost-effective choice. Solstice LBA has received U.S. Environmental Protection Agency approval under the Significant New Alternatives Policy (SNAP) Program, and is Volatile Organic Compound (VOC)-exempt per EPA.

In addition to Solstice LBA, Honeywell's family of Solstice-branded products includes refrigerants for stationary refrigeration and air conditioning applications and automotive air conditioning, gaseous blowing agents, propellants, and solvents based on Honeywell's new hydrofluoro-olefin technology that helps customers lower their carbon footprint without sacrificing end-product performance.

The products have been developed and are being commercialized by Honeywell's Fluorine Products business, a leader in the manufacture and supply of non-ozone-depleting refrigerants used by top air-conditioning and refrigeration makers worldwide, and blowing agents for energy-efficient foam insulation, as well as hydrofluoric acid and precursors for nuclear fuel.

For more information on Solstice LBA, visit www.honeywell-solsticelba.com.

Honeywell Performance Materials and Technologies is a global leader in developing and manufacturing advanced materials and process technologies. These materials and technologies are used by people every day in a wide range of industries and applications, from petroleum refining to environmentally friendlier refrigerants to bullet-resistant vests. Our advanced materials are critical in the manufacture of products ranging from nylon to computer chips to pharmaceutical packaging. Process technologies developed by our UOP business form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel and petrochemicals. UOP is now pioneering technology to produce real fuels from renewable energy sources.

Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

# # #
Media Contacts:
U.S.
Jeannine Sohayda
973-455-2706
jeannine.sohayda@honeywell.com