Check icon

Success

Your request has been successfully submitted.

Honeywell Introduces BW Clip: A New Experience In Maintenance-Free Gas Detection

Calgary, Alberta, February 11, 2015 &emdash; Honeywell (NYSE: HON), which pioneered the maintenance-free single-gas detector for the oil and gas industry, today announced the BW Clip, a new portable gas detector that makes gas detection easier, safer, more cost-effective and reliable.&emdash;The BW Clip, which will replace the industry-standard GasAlertClip Extreme, includes innovative new features, such as a hibernation case that extends service life for up to a year, an automated self-test to improve safety, and Honeywell’s exclusive SureCell™ and Reflex™ technology to ensure the gas sensor’s responsiveness and longevity, even in the harshest temperatures.The BW Clip comes in two-year versions for hydrogen sulfide, carbon monoxide, oxygen or sulfur dioxide and three-year versions for hydrogen sulfide or carbon monoxide. The maintenance-free single-gas detector runs continuously, with no need for calibration, sensor replacement, battery replacement or battery charging.“With the BW Clip, we’ve included everything that customers love about the user-friendly GasAlertClip Extreme and added new features that make gas detection easier, safer, more cost-effective and more reliable,” said Bob Fawley, product marketing manager for BW Technologies by Honeywell. “The new user-friendly hibernation case for the BW Clip can extend its service life when workers are away for extended periods of time and not using the detector,” he said. &emdash;“And thanks to the BW Clip’s automated self-test and Honeywell’s proprietary sensor technologies, companies can be confident that the detector is always monitoring for toxic gases and alerting workers to danger.” A new level of customization for maintenance-free detectorsThe BW Clip is compatible with the BW Technologies MicroDock II for automated bump testing. However, companies can get even more value from the BW Clip by using it with Honeywell’s all-new IntelliDoX instrument management system, available starting today.IntelliDoX combines smart docking modules with Honeywell’s Fleet Manager II software to provide automated testing and record-keeping for the BW Clip. The system enables companies to configure the BW Clip to fit the needs of their operation &emdash; with a level of customization not usually available in the maintenance-free detectors. To improve safety and compliance, companies can use IntelliDoX to:
  • Change the high- and low-alarm set points and other factory settings on the BW Clip, including prior to activating the detector.
  • Set a non-compliance indicator, which flashes red when a bump test is due or after a gas exposure.
  • Set other options such as a real-time clock on the BW Clip, enabling safety managers to determine the precise time of a gas event.
  • Track bump tests throughout a facility and send email notices to workers and their supervisors.
  • Easily access gas detection data via Ethernet or USB for compliance reporting.
“Most maintenance-free detectors arrive with factory settings that stay the same for the detector’s life, but with the BW Clip, customers can use IntelliDoX to configure it however they want,” said Fawley. “This way, companies have the flexibility to adjust their gas detectors to meet changing safety policies or regulations.” Faster bump testsIn addition to enabling configuration of the BW Clip, the unique design of IntelliDoX significantly accelerates functional tests, enabling companies to perform various activities for multiple BW Clip detectors &emdash; all at the same time. For example, a group of five IntelliDoX modules can bump 50 BW Clip detectors in fewer than three minutes &emdash; with no wasted calibration gas. “With the IntelliDoX, we have engineered a unique form of bump test, called the FastBump, which optimizes the functional tests, gas application and transfer of event logs from the BW Clip,” Fawley said. “Thanks to this innovation, the IntelliDoX performs the quickest bump test in the industry: five BW Clip detectors on one module in less than a minute.“With that speed, managers don’t have to set aside hours at the end of the day to bump their fleets, one detector at a time, and workers don’t have to stand in a long queue to bump their detectors,” Fawley added. “Instead, IntelliDoX prevents congestion to improve productivity, enabling plants to get more done in less time.” About HoneywellHoneywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.