Check icon

Success

Your request has been successfully submitted.

Honeywell Simplifies Healthcare IT with New Time-Saving Scanning Solution on Display Now at HIMSS

When Every Minute Counts, Easy-To-Use Mobile Technology Allows Nurses To Streamline Bedside Care FORT MILL, S.C., April 12, 2015 - As mobile devices continue to make their way into the hands of nurses across hospitals and doctor's offices, Honeywell (NYSE: HON)'s full healthcare solutions suite designed with nurses and medical professionals in mind will be on display at HIMSS, April 12-16, in booth #3017 at Chicago's McCormick Place.Designed specifically to aid nurses and medical professionals in improving their workflows, Honeywell's new Enhanced Xenon 1902h Wireless Area-Imaging Scanner, which builds upon its sixth-generation Adaptus™ area-imaging technology, is the company's newest solution to drive improved operations in patient care. Unrivaled Scanning Performance and New Nighttime Features
  • Honeywell's Xenon healthcare scanner has long been the industry-leading choice for best-in-class healthcare scanning. The new Enhanced Xenon 1902h builds upon that legacy to deliver incredibly responsive reading of virtually all 1D, PDF, and 2D bar codes and now includes a number of features specifically requested by clinicians to further enhance patient comfort and improve common clinician workflows, including the ability to quickly toggle into Patient Do-Not-Disturb and Scan Lamp modes for maximum productivity during night shifts, or when resting patients are present.
Supporting Quote
  • Jeff Fountaine, director of healthcare, Honeywell Scanning & Mobility: "Honeywell has designed new scanners for nurses and healthcare workers to improve and streamline their everyday workflow performance, making sure the technology they use offers the best care possible to patients. From specimen collection to administering medication and verifying safety protocols, our easy-to-use and quick scanners are built to simplify healthcare technology and help facilitate and support the five rights of patient safety."
The Enhanced Xenon 1920h is currently shipping globally. Supporting Resources Honeywell Scanning & Mobility (HSM) is a leading manufacturer of high-performance image- and laser-based data collection hardware, including rugged mobile computers and bar code scanners, radio frequency identification solutions, voice-enabled workflow and printing solutions. With the broadest product portfolio in the automatic identification and data collection industry, HSM provides data collection hardware for retail, healthcare, distribution centers, direct store delivery, field service and transportation and logistics companies seeking to improve operations and enhance customer service. Additionally, HSM provides advanced software, service and professional solutions that help customers effectively manage data and assets. HSM products are sold worldwide through a network of distributor and reseller partners. For more information on Honeywell Scanning & Mobility, please visit www.honeywellaidc.com.Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.Adaptus is a registered trademark or trademark of Honeywell International Inc, in the United States and or other countries.