Check icon

Success

Your request has been successfully submitted.

Honeywell to Improve Operations for Natural Gas Pipeline in China

BEIJING, July 15, 2015 Honeywell (NYSE:HON) Process Solutions (HPS) today announced that its technology will help improve operations for China's long-distance Guangxi natural gas high-pressure pipeline.A key strategic project of Sinopec Limited and Guangxi Zhuang Autonomous Region, the Guangxi pipeline is part of a liquefied natural gas (LNG) project that will play a critical role in optimizing China's energy structure and meeting the demand for natural gas in Guangxi. The project will use HPS gas measurement and equipment and software to measure the flow and pressure in the pipeline."We are able to draw upon our experience in long-distance, natural gas high-pressure pipelines to provide expertise to this essential clean energy project," said Aldous Wong, HPS vice president, Greater China. "Pipelines have challenges that are very different from processing plants since you have to manage an operation that is hundreds or sometimes thousands of miles long. Measurements such as flow and pressure must be accurate and immediately accessible to keep the pipeline operating most efficiently."The pipeline should be completed later this year, and will have a capacity of 8 billion cubic meters of natural gas a year and a total length of more than 1,300 miles, from Maoming to Beihai in the Guangxi region. This pipeline will be part of a network that transports natural gas and LNG from as far away as Kazakhstan to China. HPS technology is already being used on all three of the 1,100-mile Central Asia to China pipelines as well as the 5,600-mile West to East II pipeline across China.The integrated gas measurement technologies provided by Honeywell includes computer software and sensors that measure flow, temperature, pressure and other indicators that are critical to maintain optimum performance throughout the entire long-distance pipeline. These include:
  • Ultrasonic Flowmeters, which measure natural gas for custody transfer applications, which require high reliability, excellent metering certainty and repeatability.
  • Flow Computers, which can perform parallel calculations of compressibility according to all established methods, including GERG 88 S, AGA 8 and AGA NX 19.
  • SmartLine® Temperature and Pressure transmitters, which are the industry's first modular and most reliable transmitter, which deliver value across the entire plant lifecycle. These transmitters reduce initial purchasing costs, provide flexibility for post start-up modifications, and reduce maintenance and inventory costs while providing high accuracy and stability.
# # #Honeywell Process Solutions (www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas; refining; pulp and paper; industrial power generation; chemicals and petrochemicals; biofuels; life sciences; and metals, minerals and mining industries. Process Solutions is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes UOP, a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries.Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.comThis release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.# # #