SK Low Frequency Base Release
July 14, 2016
To satisfy specifiers' demand for more secure fire and emergency voice communications, a unique amplifier has been developed by the Silent Knight team to provide backup power capabilities for the IntelliKnight 5820XL-EVS emergency voice system.
The new line of low frequency notification solutions includes SpectrAlert® Advance low frequency sounders and sounder bases. The sounders and sounder bases are designed by System Sensor to emit a 520 Hz tone, which studies have found more effective at waking building occupants, including those with mild to severe hearing loss. The expanded line includes speakers and speaker/strobes, as well as sounder bases compatible with Silent Knight smoke, heat, and fire/carbon monoxide (CO) detectors.
These notification appliances provide the low frequency output to meet current NFPA 72 standards and International Building/Fire Code. Existing installations of current Silent Knight detectors and traditional sounder bases can be easily upgraded by replacing the base with the new low frequency version. In applications where speakers are being used for low frequency notification, the IntelliKnight 5820XL-EVS has also been updated to emit the 520 Hz tone.
Back-up power is an essential component to meeting fire alarm voice evacuation and emergency communication systems survivability requirements. The new EVS-100W can deliver 50 watts of power to the 5820XL-EVS, plus 50 watts of back-up power. For more audio power, the Silent Knight EVS-100WBU can be used for 100 watts of power with 50 watts for back-up"Survivability is a code-required function of fire and voice evac systems, and we're seeing more specs calling for more power to back-up these systems," said David Pakech, sales leader, Silent Knight-IntelliKnight. "These voice systems are getting bigger and wall space is at a premium, so the backup amp will soon be a commodity for most jobs."
More technical documentation on the SpectrAlert Advance low frequency appliances and the EVS-100W Amplifier is available on www.silentknight.com. For information on applicable low frequency requirements and emergency notification backup, visit www.silentknightblog.com. EDITORS NOTE: High- and low-resolution images associated with this press release are available in the Silent Knight image gallery.
The Silent Knight business line is part of Honeywell (NYSE: HON) Fire Safety, and designs and manufactures commercial fire alarm and life safety systems. Its broad portfolio of products is available through security equipment distribution and a nationwide network of authorized Farenhyt Distributors. Founded in 1961, Silent Knight's manufacturing operations are based in the United States. Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.