Check icon

Success

Your request has been successfully submitted.

Honeywell's Enhanced RTU2020 Process Controller Simplifies Management Of Distributed Oil And Gas Assets

HOUSTON, Nov. 12, 2015 Honeywell ( NYSE:HON) Process Solutions (HPS) today launched its newest RTU2020 process controller, which helps operating companies in oil and gas, mining and other process industries effectively manage complex remote automation and control applications.
Today's industrial operations are increasingly challenged with converting "Big Data" from complex automation systems and into relevant, actionable information. The growth of unconventional exploration and production in oil and gas has also increased the number of remote assets and data to manage. "Distributed operations are under constant pressure in all production environments. Critical assets are often widely scattered over areas where operating conditions are demanding," said Brendan Sheehan, senior marketing director, Projects and Automation Solutions, HPS. "With the RTU2020, companies have more flexibility to implement highly effective remote operations strategies across their businesses. They can benefit from reduced equipment monitoring and diagnostic time, as well as reduced travel and increased safety by not sending personnel to the field to troubleshoot device issues." The RTU2020, enhanced with native redundancy, expanded input/output (I/O) modules, and wireless I/O, is a modular process controller that provides complete visibility into the most efficient utilization of distributed assets through expanded remote monitoring, diagnostic and asset management. The unit is designed to withstand harsh environments and can be deployed at remote sites with very low power consumption (1.8 watts), which is ideal for use with solar power. It also allows for remote maintenance and cuts equipment monitoring and diagnostic time from hours to minutes. RTU2020 now increases availability through native controller redundancy no switch is required for I/O communications. A new integrated onboard solution provides wireless I/O integration of ISA100 instruments, with no specialized module needed. ISA100 instruments appear as "native" I/O to the controller. The RTU2020 controller's 28 channels of onboard I/O can now be extended by adding one or more of the new 28 channel mixed I/O modules. Like the onboard I/O, the new mixed I/O module is HART-enabled. This approach contrasts with process controllers requiring separate dedicated HART modules or external multiplexers. No extra hardware is needed with this solution, and digital HART data and diagnostics are available locally for use in control and alarming as well as remote instrument health monitoring. RTU2020's innovative design meets multi-well operational requirements in the oil and gas field, including electronic flow metering for gas per API 21.1 with per meter run licensing. Additionally, RTU2020's flow calculations have been independently validated against Alberta Energy Regulator (AER) Directive 17. ISO equations have been added to the flow calculation library alongside the existing AGA and API based calculations. Honeywell's RTU2020 offers numerous best-in-class features, including removable and plug-in terminal blocks to simplify wiring and reduce time for cabinet assembly. Integrated with Honeywell's Experion® supervisory control and data acquisition (SCADA) system, it eases configuration over thousands of assets and enables operational efficiency with an advanced human-machine interface (HMI). Users gain perfect "20/20 vision" into realizing the production potential of their distributed assets. Honeywell's distributed system architecture (DSA) allows multiple Experion SCADA servers to operate as one within a single asset or across the enterprise. Paired with Honeywell's Field Device Manager (FDM), the RTU2020 provides an effective method of remotely interrogating instrument data and diagnostics, as well as running methods like valve signatures all via the RTU2020 process controller. Honeywell Performance Materials and Technologies (PMT) is a global leader in developing advanced materials, process technologies and automation solutions. PMT's Advanced Materials businesses manufacture a wide variety of high-performance products, including environmentally friendlier refrigerants and materials used to manufacture end products such as bullet-resistant armor, nylon, computer chips and pharmaceutical packaging. Process technologies developed by PMT's UOP business ( www.uop.com) form the foundation for most of the world's refiners, efficiently producing gasoline, diesel, jet fuel, petrochemicals and renewable fuels. PMT's Process Solutions business ( www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas, refining, pulp and paper, industrial power generation, chemicals and petrochemicals, biofuels, life sciences, and metals, minerals and mining industries. Honeywell ( www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com. This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
# # #