Honeywell's Entire Family of Connected Thermostats Can Make Home More Comfortable with Amazon's Alexa-Enabled Devices
August 24, 2016
MINNEAPOLIS, Aug. 18, 2016 /PRNewswire/ -- Making sure home is comfortable should be easy, which is why every Honeywell (NYSE: HON) connected thermostat can now be controlled simply with the power of voice, using Amazon Alexa-enabled devices like Echo, thanks to a new Alexa Skill.
By simply saying "Alexa," customers with Honeywell Lyric Round' (first and second generation) or Total Connect Comfort (Wi-Fi and RedLink) thermostats can adjust their home's temperature with a short verbal command. Even homes that have multiple zones using applicable Honeywell thermostats can be adjusted, simply by confirming for Alexa which thermostat should be controlled.
The Skill is the latest collaboration between Honeywell and Amazon. Customers can also still change the temperature, set up schedules, and make other changes directly with the thermostat by using their thermostat's corresponding Honeywell app.
"Even as our homes &endash; and the tech inside them &endash; change, customers simply want to feel comfortable, safe, and in control, and find ways to save time and money," said Jeremy Eaton, General Manager, of Honeywell Connected Home. "We've always designed our thermostats with that in mind, and bringing Amazon's Alexa into our family is a perfect next step to help make people's lives easier and homes smarter."
"Every day customers are using Alexa to interact with their homes. We're excited to work with Honeywell to enable customers to control their thermostats just by asking," said Charlie Kindel, Director, Alexa Smart Home. "We're thrilled to continue to offer customers seamless ways to control their homes with Alexa."
In addition to Alexa, Honeywell's connected thermostats can be connected to other home products and ecosystems, such as Samsung SmartThings and If This Then That (IFTTT), to provide customers with the flexibility to pick solutions that best fit their needs. To learn more, please visit http://yourhome.honeywell.com. You can also follow Honeywell on Twitter (http://twitter.com/Honeywell_Home), and connect with us on Facebook (http://facebook.com/HoneywellHome).
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.