Sustainable, Energy-Efficient Communities, Home-by-Home: Honeywell's Lyric‚Ñ¢ Wi-Fi-enabled Thermostats Now Demand Response-Capable
May 11, 2017

ATLANTA, May 11, 2017 /PRNewswire/ -- A leader in home comfort and security, Honeywell (NYSE: HON) is giving consumers across the U.S. more ways to help manage their home energy use, maintain a lower carbon footprint, and create more sustainable and efficient communities.
Honeywell's full suite of Lyric™ Wi-Fi-enabled thermostats (Lyric Round, Lyric T5, and Lyric T6 Pro), are starting to be included in opt-in demand response programs with select energy and utilities providers nationwide, including those in California, New York, Texas, Massachusetts, Minnesota, Arizona, and Rhode Island.
Demand response programs are used by energy providers to avoid brownouts or blackouts during summer months when energy use exceeds their ability to deliver it to the consumer. Regional providers will be announced throughout 2017, giving consumers more convenience to maximize comfort and potential savings1 in their own connected homes.
When enrolled in a demand response program, consumers are able to conserve energy at home, while also help manage energy consumption across the larger, local area in which they live. During peak usage periods, such as when more home cooling or heating systems are running, the local energy and utilities provider can make slight adjustments to the temperature in participating homes to more efficiently use the community's available power. The U.S. Energy Information Administration has reported that residential consumers participating in a demand response program could save 100 kilowatthours on average annually2.

Consumers with Honeywell's Wi-Fi-enabled Lyric and TCC (Total Connect Comfort) thermostats are already able to use their cooling and heating systems efficiently through connected home features like app-controlled scheduling, geofencing to sense when someone is home or away, and other convenient settings. With the addition of demand response capabilities, those thermostats can further extend benefits from a single home to the larger community.
Consumers can connect with their local utilities and energy provider to find out if demand response is available in their area, and is compatible with their Honeywell thermostat; rebates on new Honeywell thermostats may also be available.
To learn more, please visit https://yourhome.honeywell.com/demandresponse/. Additional details on Honeywell's complete family of connected home products can be found at http://yourhome.honeywell.com.
You can also follow Honeywell on Twitter (http://twitter.com/Honeywell_Home), and connect with us on Facebook (http://facebook.com/HoneywellHome).
1Savings on energy bills are not guaranteed 2According to data collected by the U.S. Energy Information Administration
About Honeywell Home and Building Technologies
Honeywell Home and Building Technologies (HBT) is a global business with more than 44,000 employees worldwide. HBT creates products, software and technologies found in more than 150 million homes and 10 million buildings worldwide. We help homeowners stay connected and in control of their comfort, security and energy use. Commercial building owners and occupants use our technologies to ensure their facilities are safe, energy efficient, sustainable and productive. Our advanced metering hardware and software solutions help electricity, gas and water providers supply customers and communities more efficiently. For more news and information on Honeywell Home and Building Technologies, please visit http://www.honeywell.com/newsroom.Honeywell (www.honeywell.com) is a Fortune 100 software-industrial company that delivers industry specific solutions that include aerospace and automotive products and services; control technologies for buildings, homes, and industry; and performance materials globally. Our technologies help everything from aircraft, cars, homes and buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.