Check icon

Success

Your request has been successfully submitted.

Honeywell Rugged Mobile Computer Speeds Logistics and Manufacturing Work

Powerful new Mobility Edge device offers long operational lifecycle combined with best-in-class ruggedness

FORT MILL, S.C., June 10, 2019 – Honeywell (NYSE: HON) unveiled the CK65 Mobile Computer, which can boost supply chain productivity by streamlining and error-proofing work in distribution centers and manufacturing environments.

The rugged mobile computer offers a comprehensive software ecosystem including Honeywell’s voice-guided software, Honeywell Operational Intelligence, and a complete set of deployment utilities that integrate with popular mobile device management and enterprise mobility management solutions.

With the longest supported device lifecycle available, up to 28-hour battery life and best-in-class ruggedness, the CK65 maximizes uptime while providing an easy path for users migrating from legacy Windows® operating systems to the AndroidTM platform.

The CK65 is built on Honeywell’s Mobility Edge platform, a unified hardware and software architecture with an integrated software toolset that extends asset life, accelerates deployment and simplifies management of mobility solutions. The only platform that guarantees support through Android R, Mobility Edge enables IT departments to reuse their investment in solution development and software certification across multiple computer form factors.

With a Honeywell Edge Services contract including five years of SentinelTM security patches, CK65 users can expect secure, productive use through 2028.

The mobile computer is ideal for applications across the logistics and manufacturing sectors, including receiving, put-away, cross docking, shipping accuracy, parts/material/work in progress tracking and inventory management.

“Built on the Mobility Edge platform, the CK65 is the next generation in Honeywell’s long legacy of providing industry-leading ruggedized mobile computers for the warehouse,” said Michael Noyes, vice president for Mobility, Scan and Print for Honeywell’s Productivity Products business. “The CK65, along with Honeywell Edge Services, is designed to maximize productivity and uptime while reducing the cost to support, providing the solutions customers investing in handheld devices need.”

 

An Ideal Platform for Android-Based Solutions

Many warehouse operators are now faced with the challenge of migrating from legacy Windows devices to Android.

Honeywell and its partners provide support for new Android application development and Windows-to-Android migration. Starting with a concept and design workshop, users can get help with development, test, implementation, deployment and support of Android-based solutions, whether migrating from Windows or starting from scratch.

The mobile computer is backward-compatible with accessories owned by users of Honeywell’s popular CK3X and CK3R mobile computers, and easily adaptable to FlexDockTM accessories owned by users of CK71 and CK75 computers.

The CK65 is validated by Android Enterprise Recommended, a Google-led initiative that helps businesses confidently select, deploy, and manage Android devices and services best suited to their enterprise needs.

 

Extensive Software Ecosystem

The CK65 comes with a pre-installed software client pack including a secure enterprise browser, application launcher and pre-licensed, Honeywell SmartTE powered by StayLinked terminal emulation software.

SmartTE ensures high speed, secure access to back-end warehouse management system software while virtually eliminating dropped sessions during interruptions such as shift changes, network issues and battery replacements. The software can enhance productivity by transforming "green screens" into easy-to-use, graphical user interfaces with no changes to the underlying enterprise application.

The mobile computer supports Honeywell’s Guided Work Solutions, based on the company’s industry-leading Vocollect voice technology. The worker-focused software can be integrated with multiple enterprise resource planning platforms for distribution centers of all sizes.

The CK65 can be connected to Honeywell Operational Intelligence, an intuitive, cloud-based software solution that systematically tracks, manages and optimizes mobile computers – across all locations – throughout the operational lifecycle, simplifying the return-to-manufacturer authorization process.

By leveraging the capabilities of the Mobility Edge platform and edge machine learning, Operational Intelligence will detect, log and report abnormal fall and impact events during operations, helping users to maximize the life of the physical asset.

Guided Work Solutions, Operational Intelligence and other leading software applications can be downloaded through the Honeywell Marketplace, an enterprise app store designed to provide businesses with direct access to software and solutions developed by Honeywell and third-party partners. The Honeywell Marketplace is designed to be the leading place for enterprises to find innovative solutions, technologies and services to meet their internal or customer’s strategic needs.

 

Advanced Hardware Platform

The CK65’s hardware design minimizes cost of ownership by reducing downtime. It is the most rugged device in its class, surviving drops of 8 feet to concrete across the operating temperature range. The 7,000 mAh battery allows the CK65 to run for 28 hours between battery changes in representative tests, further reducing downtime.

The CK65 features a 7th-generation scan engine delivering exceptional speed and motion tolerance. With standard and long-range options, the CK65 reads a complete range of linear and 2D codes, including, with additional software dot peen and laser-etched direct-parts-marked codes employed in automotive and other manufacturing environments.

Android is a trademark or registered trademark of Google, Inc. in the United States and/or other countries.

Mobility Edge is a trademark of Honeywell International Inc. in the United States and/or other countries.

Honeywell Safety and Productivity Solutions (SPS) provides products, software and connected solutions that improve productivity, workplace safety and asset performance for our customers across the globe. We deliver on this promise through industry-leading mobile devices, software, cloud technology and automation solutions, the broadest range of personal protective equipment and gas detection technology, and custom-engineered sensors, switches and controls. We also manufacture and sell a broad portfolio of footwear for work, play and outdoor activities, including XtraTufTM and Muck BootTM brand footwear.

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help everything from aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable.  For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Whitney Ellis
Retail