The Rise of Warehouse Automation

Today, warehouses require high operational speed, accuracy, and efficiency to survive. Major trends such as e-commerce have raised customer expectations to new heights. According to Statista, the e-commerce market in the United States is forecast to grow by 51% over the next four years and is estimated to reach $1.1 trillion by 2029. Especially on the consumer side, the option for next-day delivery of ordered products is becoming more commonplace. These trends significantly burden the warehouse industry, and the need to process higher volumes of goods at faster rates has been made more difficult due to severe labor shortages. A recent Hanover Research/Berkshire Grey survey reveals that 57% of executives believe labor shortages have hindered their ability to meet demand. To overcome these challenges, warehouses must continue modernizing to remain competitive. Many are searching for future-proof automation software solutions. However, making the right choice can be complex and fraught with risk. Fortunately, innovations in automation now offer a lifeline to organizations struggling to keep up.

Download Whitepaper