Built for Capacity and Compliance: Developing Data Centers in Georgia
Georgia’s data center boom is accelerating. Discover key considerations for developers, from AI-driven demand and tax incentives to utility costs, compliance, and growth planning.
Georgia has become one of the fastest-growing data center markets in the United States. Rapidly rising demand for AI infrastructure, combined with the state’s land availability, connectivity and tax incentives, are all contributing factors to Georgia’s accelerating development. As growth continues, however, capacity is only part of the equation. Developers must also address utility cost allocation, reporting, tax qualification and increasingly localized development controls—often before a new campus design is finalized.
Power rules are changing the development calculus
Recent large-load rules adopted by the Georgia Public Service Commission (PSC) in 2025 have changed the development across the state. For projects above 100 MW, customized utility terms may include 15-year contracts, minimum bills and recovery of site-specific and upstream generation, transmission and distribution costs, with qualifying contracts subject to PSC review[i]. Decision makers should therefore treat credible load forecasting, demand flexibility and grid-responsible operations as core elements of site selection and capital planning—not just as part of an interconnection request.
This scrutiny reflects a dramatic shift in planning. Georgia Power’s seven-year generation estimate rose from 400 MW in 2022 to 8,500 MW two years later, according to the PSC[ii]. The commission also requires quarterly data center reporting and cost-allocation studies intended to keep growth costs from shifting to existing customers[iii].
Transparency, tax qualification and local control add complexity
Proposed Senate Bill 421—the “Data Center Transparency Act”—would prevent Georgia local governments and authorities from entering agreements that bar disclosure of an entity’s electricity or water use[iv]. At the same time, cities and counties may impose their own zoning, siting and development conditions[v]. Early, defensible data on energy, water and operational performance can therefore support both regulatory submissions and community engagement.
Georgia’s high-technology data center equipment exemption also requires proof that statutory investment and new-quality-job thresholds can be met. Treating incentives, utility obligations and local approvals as connected workstreams can help reduce late-stage redesign and documentation gaps.
Turn compliance data into an operating advantage
Partnering with Honeywell Technologies early can help teams establish the digital and energy-management foundation needed for permitting, utility coordination and long-term operations. Honeywell Technologies Forge Sustainability+ for Buildings can integrate energy data, track consumption, utility costs and Scope 1 and 2 emissions, and provide reporting with export flexibility. While Honeywell Technologies Power Manager can help optimize on-site supply resources and building assets from design through operation based on grid availability, utility rates and energy consumption.
Together, these capabilities can improve load visibility, support demand and resilience planning, and provide an adaptable reporting model as Georgia’s requirements evolve. The result is infrastructure designed not only for capacity, but also for compliance, transparency and operational efficiency.
Simplify your path from concept to operation. Connect with Honeywell Technologies to explore an early-stage data center strategy for Georgia.
-
Utility MeteringSeconds that save lives
Improve life safety and security with Honeywell Technologies' connected monitoring and predictive analytics to detect utility risks faster and protect critical assets.
-
Utility MeteringBuilding a culture of safety
Build a stronger utility safety culture with connected data, smart meters and predictive insights that help prevent incidents and speed recovery.
-
Operational EfficiencyMore Than Six Decades of Trusted Thermal Sensing: The Honeywell Ongoing Partnership with Boeing
While advances in aviation technology continue to accelerate, one thing remains constant: the need for precise, dependable temperature control throughout an aircraft. For more than six decades, Honeywell has supplied bimetal thermostats and temperature sensing solutions that help monitor temperatures in critical systems.
-
AIHoneywell Productivity Solutions and Services (PSS) MODEX 2026 Recap
Discover key supply chain trends from MODEX 2026, including AI-driven operations, warehouse automation, real-time intelligence, and connected technologies transforming logistics and fulfillment.
- Show More
Footnotes:
[i] Georgia Public Service Commission “PSC Approves Rule to Allow New Power Usage Terms for Data Centers,” Jan. 25, 2025, [September 2026].
[ii] Georgia Public Service Commission, “Data Center Fact Sheet,” Sept. 2026 [Accessed Sept. 2026].
[iii] Georgia Public Service Commission, “Data Center Fact Sheet,” Sept. 2026 [Accessed Sept. 2026].
[iv] Zoe Seiler, “Georgia lawmakers debating data center moratorium and regulation bills in legislature,” WABE, Feb. 17, 2026, [September 2026].
[v] You, Yang, “Georgia Data Center Hub,” [September 2026].