Modular Equipment Allows Indonesian Natural Gas
Honeywell UOP Modular Equipment allows Indonesian Natural Gas Producer to Fuel Wellhead Equipment
Honeywell UOP Modular Equipment allows Indonesian Natural Gas Producer to Fuel Wellhead Equipment
DES PLAINES, Ill., Sept. 14, 2016 — Honeywell (NYSE: HON) UOP today announced that its modular natural gas processing equipment enables Virginia Indonesia Company (VICO) to use natural gas straight from the wellhead to power on-site equipment.
Raw natural gas is often corrosive, or “sour,” making it unsuitable for fueling on-site power-generation machinery without damaging the equipment. The modular fuel gas conditioning system uses Honeywell UOP’s Separex™ technology to remove corrosive contaminants from natural gas streams, allowing it to safely and reliably fuel on-site machinery.
“Honeywell UOP’s modular Separex technology is factory-built, easily shipped to the project site and ideally suited for operation in remote locations,” said John Gugel, vice president and general manager for Honeywell UOP’s Gas Processing and Hydrogen business. “The value of this solution is that you can use the very fuel you’re producing to run the on-site equipment, rather than another fuel such as diesel that continually has to be transported to the site and is subject to supply interruptions.”
Because it is built in a factory, the system starts up faster and operates more reliably than systems constructed on site, enabling customers to begin earning revenue faster. The standardized modular system is designed to easily fit together with other equipment and is easier to operate due to common parts and standardized training, operations and maintenance.
Demand for natural gas is rising in Indonesia and many other developing countries along with economic growth, even as domestic sources of crude oil decline by about 4 percent annually. The government of Indonesia is making infrastructure investments to promote the use of natural gas as a transportation and household fuel, a feedstock for fertilizers, and for generating electricity.
The Indonesia natural gas program includes the development of new domestic sources to forestall importation, which could become necessary as early as 2019, according to the nation’s Ministry of Energy and Mineral Resources. Indonesia currently has proven reserves of 98 trillion standard cubic feet (TSCF) of natural gas, with as many as 53 TSCF yet to be developed, according to the Ministry.
Rapid commercialization of new gas reserves in Indonesia will require substantial investment as part of a $24 billion national energy modernization program that will bring natural gas from distant locations to population centers in Java and Sumatra. Modular equipment from Honeywell UOP is critical to powering and processing natural gas at wells in these remote areas.
Honeywell UOP Separex membrane systems contain spiral wound membrane elements that remove acid gas and water from natural gas streams. Decades of operation in natural gas service demonstrate that Separex membranes are the most durable type of membrane in the industry. To date, more than 130 Separex systems have been installed worldwide.
“This application of the technology is in a remote location in Indonesia, proving that it can be a viable solution just about anywhere in the world where sour gas is available to run equipment,” Gugel said. “Modular units such as this are built to very high standards in a controlled environment and can even be redeployed to other locations if necessary.”
VICO has operated the Sanga-Sanga Production Sharing Contract (PSC), located in the Kutai Basin of East Kalimantan, for more than 40 years. It has produced more than 12.6 TSCF of gas and 0.4 billion barrels of liquid from the production fields in Badak, Mutiara, Semberah, Nilam, Pamaguan, Lampake, and Beras.
Honeywell UOP (www.uop.com) is a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is part of Honeywell’s Performance Materials and Technologies strategic business group, which also includes Honeywell Process Solutions (www.honeywellprocess.com), a pioneer in automation control, instrumentation and services for the oil and gas, refining, petrochemical, chemical and other industries.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services, and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments, and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
# # #
Contact:
John Simley
847-391-2278
john.simley@honeywell.com