Honeywell Releases Wireless Combination Smoke And Carbon Monoxide Detector

Honeywell Releases Wireless Combination Smoke And Carbon Monoxide Detector

MELVILLE, N.Y., March 29, 2017 – Honeywell (NYSE: HON) today released its first-ever professionally installed and monitored wireless combination smoke and carbon monoxide (CO) detector for homes. The 5800COMBO is easy for dealers to install and helps to protect homeowners from multiple dangers through continuous central station monitoring, compared to unmonitored detectors. The battery-powered 5800COMBO contains a built-in transmitter that allows central stations outside the home to monitor alarm events in the home – such as smoke and CO gas – as well as monitor for maintenance conditions. It alerts occupants to the danger and transmits a smoke or CO alarm signal to the panel when smoke is detected or when specified levels of CO are reached in the home. “This detector provides a high level of false alarm immunity while quickly reacting to smoldering fire – that kind of accuracy is critical when it comes to saving lives,” said Mark Okeefe, product marketing manager, security and fire, Honeywell Home and Building Technologies. “This gives the dealer an easier path to offering dual capabilities in a single device, and more importantly, helps meet the needs of the consumer.” The device uses both voice and visual display to alert occupants. Voice notifies the occupant of the threat and announces what action should be taken. A multi-color LED light ring is visible from all sides and angles, providing visual annunciation when there is danger. For example, a smoke alarm condition illuminates red, a CO alarm condition illuminates blue and a tri-color status light indicates operating mode or if there is a maintenance condition that requires attention. Additionally, a built-in sounder provides audible annunciation with Temporal 3 or Temporal 4 alarm tones. These visual and audible cues intuitively help the user to quickly identify the alarm event for a rapid response. From a technical perspective, the 5800COMBO uses a number of sensors to distinguish a real fire from a nuisance issue, such as burning toast. A photoelectric chamber senses airborne smoke particulates; its electrochemical sensor monitors for CO, a bi-product produced by slow smoldering fires; and an infrared flame sensor measures ambient light levels and flame signatures while thermal detection monitors for a rise in temperature. Automatic drift compensation and smoothing algorithms accommodate for dust build-up over time. These, along with a 10-year life CO sensor, help provide years of reliable service. The 5800COMBO works with all Honeywell Security and Fire security platforms, including VISTA ®,  LYNX and Lyric ®. For more information, please visit https://www.security.honeywell.com

About Honeywell Home and Building Technologies

Honeywell Home and Building Technologies (HBT) is a global business with more than 44,000 employees worldwide. HBT creates products, software and technologies found in more than 150 million homes and 10 million buildings worldwide. We help homeowners stay connected and in control of their comfort, security and energy use. Commercial building owners and occupants use our technologies to ensure their facilities are safe, energy efficient, sustainable and productive. Our advanced metering hardware and software solutions help electricity, gas and water providers supply customers and communities more efficiently. For more news and information on Honeywell Home and Building Technologies, please visit https://www.honeywell.com/us/en/news.

Honeywell (www.honeywell.com/us/en) is a Fortune 100 software-industrial company that delivers industry specific solutions that include aerospace and automotive products and services; control technologies for buildings, homes, and industry; and performance materials globally. Our technologies help everything from aircraft, cars, homes and buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/us/en/news.